AngleTolerance |
Returns or sets the tolerance, in degrees, used to determine when angles are zero. |
BoundaryPlane |
Returns or sets the plane defined to indicate the boundary of the plate system. |
BoundarySection |
Returns the section containing curves that define the boundary of the plate system. |
BoundarySheets |
Returns the sheet bodies or datum planes selected, or a face collector used to define the boundary of the plate system. |
DistanceTolerance |
Returns or sets the tolerance used to determine when distances are considered zero. |
Offset |
Returns the offset to apply to the selected mold face to produce the desired mold face. |
OrientationAngleRule |
Returns or sets the angle rule to use when measuring angles. |
ParentFeatureInternal |
Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag |
Returns or sets the patch solution flag |
PatchSurfaceFilename |
Returns or sets the patch surface filename |
Primary |
Returns or sets the primary stiffener direction. |
PrimaryOnReference |
Returns or sets the primary stiffener direction when the plate system is located on a midship reference. |
ProjectionDirection |
Returns the direction used to project the boundary section curves onto the mold face. |
Regions |
Returns the regions selected from the sheet, that has the inscribed boundaries, to keep for the final plate system shape. |
Secondary1 |
Returns or sets the direction of the stiffener flange. |
Secondary1OnReference |
Returns or sets the direction of the stiffener flange when the stiffener is located on a midship reference. |
Secondary2 |
Returns or sets the direction of the stiffener flange. |
Secondary2OnReference |
Returns or sets the direction of the stiffener flange when the stiffener is located on a midship reference. |
ShipNames |
Returns the Ship Names builder, used to assign names to the Plate Systems created. |
SplitKnuckleEdges |
Returns the split knuckle edges, which are used to create seam feature to split a plate system into plate subsystem. |
Stock |
Returns the plate stock builder, used to define the plate material, grade, thickness, mass density, and thicken option. |
SurroundingPatchSurfaceFilename |
Returns or sets the surrounding patch surface filename |
Tag |
Returns the Tag for this object. |
ThicknessDirection |
Returns the thickness direction builder, used to specify the thickness direction from the mold face. |
Tightness |
Returns or sets the tightness desired for the plate system. |
Weld |
Returns the welding characteristics builder, used to assign welding characteristics to the outermost edges of a plate system. |