PillarSystemBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
PillarSystemBuilder
¶ Bases:
NXOpen.Features.ShipDesign.ProfileSystemBuilder
Represents a
NXOpen.Features.ShipDesign.PillarSystem
builder which is used to create or edit a pillar system feature.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreatePillarSystemBuilder()
Default values.
Property Value OrientationAngle.Value 0 SectionType Profile New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AnchorPoint | Returns or sets the anchor point. |
AngleTolerance | Returns or sets the tolerance, in degrees, used to determine when angles are zero. |
Boundary1 | Returns the collector containing the plate system, profile system, or datum plane that will be used to trim the first end of the generated profile system. |
Boundary1Plane | Returns or sets the defined plane that will be used to trim the first end of the generated profile system. |
Boundary2 | Returns the collector containing the plate system, profile system, or datum plane that will be used to trim the second end of the generated profile system. |
Boundary2Plane | Returns or sets the defined plane that will be used to trim the second end of the generated profile system. |
BoundaryReverse | Returns or sets the indication if the side of a single boundary should be changed to the other side or not. |
BuildSolid | Returns or sets the indication of whether to build a solid for the pillar system or just the curve. |
BuiltUpStock | Returns the stock used to build the builtUp from. |
Direction | Returns or sets the direction of the pillar. |
DistanceTolerance | Returns or sets the tolerance used to determine when distances are considered zero. |
FirstIntersectionPoints | Returns the selected intersection points between the curves and the first boundary. |
IntersectingShipStructure | Returns the ship structure to intersect with each other that defines the start of a pillar. |
LimitingShipStructure | Returns the ship sructure that defines the end of the pillar. |
OrientationAngle | Returns the angle at which to orient the stock shape. |
OrientationAngleRule | Returns or sets the angle rule to use when measuring angles. |
OrientationLine | Returns the orientation line, used only if the creation method is Specify Line. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PointPairList | Returns the list of pairs of points that define the ends of the pillars. |
ReverseOrientationDirection | Returns or sets the reverse orientation direction |
ReversePathDirection | Returns or sets the flag that indicates if the default curve direction should be reversed or not. |
ReverseReferenceDirection | Returns or sets the reverse reference direction |
SecondIntersectionPoints | Returns the selected intersection points between the curves and the second boundary. |
SectionType | Returns or sets the section type (profile or plate) |
ShipNames | Returns the Ship Names builder, used to assign names to the Pillar Systems created. |
SplitKnuckleLocations | Returns the collector containing the knuckle points that are to be used to create seams. |
StockData | Returns the stock data used to define the stock information of the stiffener. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of input used to define the pillar location. |
UseNewDefaultSectionAlgorithm | Returns or sets the flag that indicates if the new default section algorithm is used. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreatePathCurves | Creates path curves for all the paths of the profile system. |
CreatePlaneForList | Create a NXOpen.Features.ShipDesign.PlaneListBuilder to add a defined plane to a list. |
CreatePointPairBuilder | Creates a NXOpen.Features.ShipDesign.PointPairBuilder . |
DeleteLastPathCurves | Deletes the path curves returned from a call to GetLastPathCurves() . |
DeletePathCurves | Deletes the path curves created from a call to CreatePathCurves() . |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAvailableAnchorPointNames | The list of available anchor points |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetLastPathCurves | Gets the path curves used by NXOpen.Features.ShipDesign.OrientationDefinitionBuilder . |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
PopulateAnchorPointList | Update anchor points |
SetBoundaryOnePoints | Sets the selected intersection points for the first boundary. |
SetBoundaryTwoPoints | Set the selected intersection points for the second boundary. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetRegionPoints | Sets the points that identify which regions of the curves will be used. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PillarSystemBuilderStockSectionType Enumeration | SpreadSheet Type Profile or BuiltUp |
PillarSystemBuilderTypes Enumeration | Used to specify how the pillar system is defined. |
Property Detail¶
AnchorPoint¶
-
PillarSystemBuilder.
AnchorPoint
¶ Returns or sets the anchor point.
-------------------------------------
Getter Method
Signature
AnchorPoint
Returns: Return type: int New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnchorPoint
Parameters: anchorPoint (int) – New in version NX9.0.3.
License requirements: nx_ship_basic (“Ship Basic Design”)
BuildSolid¶
-
PillarSystemBuilder.
BuildSolid
¶ Returns or sets the indication of whether to build a solid for the pillar system or just the curve.
-------------------------------------
Getter Method
Signature
BuildSolid
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BuildSolid
Parameters: buildSolid (bool) – New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
BuiltUpStock¶
-
PillarSystemBuilder.
BuiltUpStock
¶ Returns the stock used to build the builtUp from.
-------------------------------------
Getter Method
Signature
BuiltUpStock
Returns: Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX9.0.0.
License requirements: None.
Direction¶
-
PillarSystemBuilder.
Direction
¶ Returns or sets the direction of the pillar.
Only used when Type is Features.ShipDesign.PillarSystemBuilder.Types.ShipStructure.
-------------------------------------
Getter Method
Signature
Direction
Returns: Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction
Parameters: direction ( NXOpen.Direction
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
IntersectingShipStructure¶
-
PillarSystemBuilder.
IntersectingShipStructure
¶ Returns the ship structure to intersect with each other that defines the start of a pillar.
Only used when Type is Features.ShipDesign.PillarSystemBuilder.Types.ShipStructure.
-------------------------------------
Getter Method
Signature
IntersectingShipStructure
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
LimitingShipStructure¶
-
PillarSystemBuilder.
LimitingShipStructure
¶ Returns the ship sructure that defines the end of the pillar.
Only used when Type is Features.ShipDesign.PillarSystemBuilder.Types.ShipStructure.
-------------------------------------
Getter Method
Signature
LimitingShipStructure
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
OrientationAngle¶
-
PillarSystemBuilder.
OrientationAngle
¶ Returns the angle at which to orient the stock shape.
-------------------------------------
Getter Method
Signature
OrientationAngle
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OrientationLine¶
-
PillarSystemBuilder.
OrientationLine
¶ Returns the orientation line, used only if the creation method is “Specify Line”.
-------------------------------------
Getter Method
Signature
OrientationLine
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX8.5.0.
License requirements: None.
PointPairList¶
-
PillarSystemBuilder.
PointPairList
¶ Returns the list of pairs of points that define the ends of the pillars.
Only used when Type is Features.ShipDesign.PillarSystemBuilder.Types.Points.
-------------------------------------
Getter Method
Signature
PointPairList
Returns: Return type: NXOpen.NXObjectList
New in version NX8.0.0.
License requirements: None.
ReverseOrientationDirection¶
-
PillarSystemBuilder.
ReverseOrientationDirection
¶ Returns or sets the reverse orientation direction
-------------------------------------
Getter Method
Signature
ReverseOrientationDirection
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseOrientationDirection
Parameters: reverseOrientationDirection (bool) – New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
ReverseReferenceDirection¶
-
PillarSystemBuilder.
ReverseReferenceDirection
¶ Returns or sets the reverse reference direction
-------------------------------------
Getter Method
Signature
ReverseReferenceDirection
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseReferenceDirection
Parameters: reverseReferenceDirection (bool) – New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
SectionType¶
-
PillarSystemBuilder.
SectionType
¶ Returns or sets the section type (profile or plate)
-------------------------------------
Getter Method
Signature
SectionType
Returns: Return type: NXOpen.Features.ShipDesign.PillarSystemBuilderStockSectionType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionType
Parameters: sectionType ( NXOpen.Features.ShipDesign.PillarSystemBuilderStockSectionType
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
ShipNames¶
-
PillarSystemBuilder.
ShipNames
¶ Returns the Ship Names builder, used to assign names to the Pillar Systems created.
-------------------------------------
Getter Method
Signature
ShipNames
Returns: Ship Names Builder Return type: NXOpen.Features.ShipDesign.ShipNamesBuilder
New in version NX9.0.2.
License requirements: None.
StockData¶
-
PillarSystemBuilder.
StockData
¶ Returns the stock data used to define the stock information of the stiffener.
-------------------------------------
Getter Method
Signature
StockData
Returns: Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX8.0.0.
License requirements: None.
Type¶
-
PillarSystemBuilder.
Type
¶ Returns or sets the type of input used to define the pillar location.
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.ShipDesign.PillarSystemBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.ShipDesign.PillarSystemBuilderTypes
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Method Detail¶
CreatePointPairBuilder¶
-
PillarSystemBuilder.
CreatePointPairBuilder
¶ Creates a
NXOpen.Features.ShipDesign.PointPairBuilder
.Signature
CreatePointPairBuilder()
Returns: Return type: NXOpen.Features.ShipDesign.PointPairBuilder
New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
GetAvailableAnchorPointNames¶
-
PillarSystemBuilder.
GetAvailableAnchorPointNames
¶ The list of available anchor points
Signature
GetAvailableAnchorPointNames()
Returns: Array of available anchor point names. These names are read from the current reuse sketch :rtype: list of str
New in version NX9.0.3.
License requirements: None.
PopulateAnchorPointList¶
-
PillarSystemBuilder.
PopulateAnchorPointList
¶ Update anchor points
Signature
PopulateAnchorPointList()
New in version NX9.0.3.
License requirements: None.
Validate¶
-
PillarSystemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.