ManufacturingPreparationBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ManufacturingPreparationBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
This builder is used to adds attributes to the part and body identifying manufacturing related data.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateManufacturingPreparationBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AftStiffenerExtension | Returns the aft stiffener extension. |
AssemblyComponent | Returns the assembly part to add components to |
FeatureName | Returns or sets the feature name |
ForwardStiffenerExtension | Returns the forward stiffener extension. |
Mirror | Returns or sets the mirror option |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReassignPositionNumbers | Returns or sets the reassign position numbers toggle |
ReferenceFeatureName | Returns or sets the feature name |
SaProject | Returns or sets the project number assigned to the ship. |
SeamingObjects | Returns the objects that define straking seams |
SectionNumber | Returns or sets the ship section number. |
SteelComponents | Returns the design elements to prepare for manufacturing. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Trim | Returns or sets the trim option |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FindIntersectingParts | The design parts that intersect the manufacturing collector |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetComponentSeams | The seams to load for the component |
GetDesignElementAttributeValue | Get the attribute value of the given design element. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
InitializeDesignElementAttributes | Read the design attributes and use them to initialize the builder values. |
SetDesignElementAttributeValue | Set the attribute value of the given design element. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
UpdateSeamsMap | The seams map for the selected components. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ManufacturingPreparationBuilderAttributeType Enumeration | Represents manufacturing attribute type. |
Property Detail¶
AftStiffenerExtension¶
-
ManufacturingPreparationBuilder.
AftStiffenerExtension
¶ Returns the aft stiffener extension.
-------------------------------------
Getter Method
Signature
AftStiffenerExtension
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
AssemblyComponent¶
-
ManufacturingPreparationBuilder.
AssemblyComponent
¶ Returns the assembly part to add components to
-------------------------------------
Getter Method
Signature
AssemblyComponent
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX10.0.1.
License requirements: None.
FeatureName¶
-
ManufacturingPreparationBuilder.
FeatureName
¶ Returns or sets the feature name
-------------------------------------
Getter Method
Signature
FeatureName
Returns: Return type: str New in version NX8.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureName
Parameters: featureName (str) – New in version NX8.0.3.
License requirements: nx_ship_concept (“Ship Concept”)
ForwardStiffenerExtension¶
-
ManufacturingPreparationBuilder.
ForwardStiffenerExtension
¶ Returns the forward stiffener extension.
-------------------------------------
Getter Method
Signature
ForwardStiffenerExtension
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Mirror¶
-
ManufacturingPreparationBuilder.
Mirror
¶ Returns or sets the mirror option
-------------------------------------
Getter Method
Signature
Mirror
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Mirror
Parameters: mirror (bool) – New in version NX11.0.0.
License requirements: None.
ReassignPositionNumbers¶
-
ManufacturingPreparationBuilder.
ReassignPositionNumbers
¶ Returns or sets the reassign position numbers toggle
-------------------------------------
Getter Method
Signature
ReassignPositionNumbers
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReassignPositionNumbers
Parameters: reassign (bool) – New in version NX11.0.1.
License requirements: None.
ReferenceFeatureName¶
-
ManufacturingPreparationBuilder.
ReferenceFeatureName
¶ Returns or sets the feature name
-------------------------------------
Getter Method
Signature
ReferenceFeatureName
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceFeatureName
Parameters: featureName (str) – New in version NX11.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
SaProject¶
-
ManufacturingPreparationBuilder.
SaProject
¶ Returns or sets the project number assigned to the ship.
-------------------------------------
Getter Method
Signature
SaProject
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaProject
Parameters: saProject (str) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
SeamingObjects¶
-
ManufacturingPreparationBuilder.
SeamingObjects
¶ Returns the objects that define straking seams
-------------------------------------
Getter Method
Signature
SeamingObjects
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX10.0.1.
License requirements: None.
SectionNumber¶
-
ManufacturingPreparationBuilder.
SectionNumber
¶ Returns or sets the ship section number.
-------------------------------------
Getter Method
Signature
SectionNumber
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionNumber
Parameters: sectionNumber (str) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
SteelComponents¶
-
ManufacturingPreparationBuilder.
SteelComponents
¶ Returns the design elements to prepare for manufacturing.
-------------------------------------
Getter Method
Signature
SteelComponents
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX8.0.0.
License requirements: None.
Trim¶
-
ManufacturingPreparationBuilder.
Trim
¶ Returns or sets the trim option
-------------------------------------
Getter Method
Signature
Trim
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Trim
Parameters: trim (bool) – New in version NX11.0.0.
License requirements: None.
Method Detail¶
FindIntersectingParts¶
-
ManufacturingPreparationBuilder.
FindIntersectingParts
¶ The design parts that intersect the manufacturing collector
Signature
FindIntersectingParts()
Returns: Return type: list of NXOpen.Assemblies.Component
New in version NX10.0.1.
License requirements: None.
GetComponentSeams¶
-
ManufacturingPreparationBuilder.
GetComponentSeams
¶ The seams to load for the component
Signature
GetComponentSeams(selectedComp)
Parameters: selectedComp (int) – New in version NX10.0.1.
License requirements: nx_ship_concept (“Ship Concept”)
GetDesignElementAttributeValue¶
-
ManufacturingPreparationBuilder.
GetDesignElementAttributeValue
¶ Get the attribute value of the given design element.
Signature
GetDesignElementAttributeValue(designElement, attrType)
Parameters: - designElement (
NXOpen.DisplayableObject
) – the design element for manufacturing preparation. - attrType (
NXOpen.Features.ShipDesign.ManufacturingPreparationBuilderAttributeType
) – the attriubte type.
Returns: the attribute value.
Return type: str
New in version NX8.0.0.
License requirements: None.
- designElement (
InitializeDesignElementAttributes¶
-
ManufacturingPreparationBuilder.
InitializeDesignElementAttributes
¶ Read the design attributes and use them to initialize the builder values.
Signature
InitializeDesignElementAttributes(designElement)
Parameters: designElement ( NXOpen.DisplayableObject
) – the design element for manufacturing preparation.New in version NX8.0.0.
License requirements: None.
SetDesignElementAttributeValue¶
-
ManufacturingPreparationBuilder.
SetDesignElementAttributeValue
¶ Set the attribute value of the given design element.
Signature
SetDesignElementAttributeValue(designElement, attrType, attrValue)
Parameters: - designElement (
NXOpen.DisplayableObject
) – the design element for manufacturing preparation. - attrType (
NXOpen.Features.ShipDesign.ManufacturingPreparationBuilderAttributeType
) – the attriubte type. - attrValue (str) – the attribute value.
New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
- designElement (
UpdateSeamsMap¶
-
ManufacturingPreparationBuilder.
UpdateSeamsMap
¶ The seams map for the selected components.
Signature
UpdateSeamsMap(selectedComps)
Parameters: selectedComps (list of int) – New in version NX10.0.1.
License requirements: nx_ship_concept (“Ship Concept”)
Validate¶
-
ManufacturingPreparationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.