MainDimensionsBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
MainDimensionsBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.MainDimensions
builder.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateMainDimensionsBuilder()
Default values.
Property Value AftPerpendicular.Value 0 (millimeters part), 0 (inches part) Baseline.Value 0 (millimeters part), 0 (inches part) ForwardPerpendicular.Value 0 (millimeters part), 0 (inches part) Midship.Value 0 (millimeters part), 0 (inches part) Waterline.Value 0 (millimeters part), 0 (inches part) XMax.Value 25000 (millimeters part), 1000 (inches part) XMin.Value 0 (millimeters part), 0 (inches part) YMax.Value 2500 (millimeters part), 100 (inches part) ZMax.Value 2500 (millimeters part), 100 (inches part) ZMin.Value 0 (millimeters part), 0 (inches part) New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AftPerpendicular | Returns the expression containing the position value of Aft Perpendicular along the X axis. |
Baseline | Returns the expression containing the position value of baseline along the Z axis. |
ForwardPerpendicular | Returns the expression containing the position value of forward Perpendicular along the X axis. |
GridID | Returns or sets the unique Grid ID for each ship. |
Midship | Returns the expression containing the position value of midship along the X axis. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ShipBody | Returns the ship body. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Waterline | Returns the expression containing the position value of waterline along the Z axis. |
XMax | Returns the expression containing the x max value. |
XMin | Returns the expression containing the x min value. |
YMax | Returns the expression containing the y max value. |
ZMax | Returns the expression containing the z max value. |
ZMin | Returns the expression containing the z min value. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AftPerpendicular¶
-
MainDimensionsBuilder.
AftPerpendicular
¶ Returns the expression containing the position value of Aft Perpendicular along the X axis.
-------------------------------------
Getter Method
Signature
AftPerpendicular
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Baseline¶
-
MainDimensionsBuilder.
Baseline
¶ Returns the expression containing the position value of baseline along the Z axis.
-------------------------------------
Getter Method
Signature
Baseline
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ForwardPerpendicular¶
-
MainDimensionsBuilder.
ForwardPerpendicular
¶ Returns the expression containing the position value of forward Perpendicular along the X axis.
-------------------------------------
Getter Method
Signature
ForwardPerpendicular
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
GridID¶
-
MainDimensionsBuilder.
GridID
¶ Returns or sets the unique “Grid ID” for each ship.
-------------------------------------
Getter Method
Signature
GridID
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridID
Parameters: gridID (str) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Midship¶
-
MainDimensionsBuilder.
Midship
¶ Returns the expression containing the position value of midship along the X axis.
-------------------------------------
Getter Method
Signature
Midship
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ShipBody¶
-
MainDimensionsBuilder.
ShipBody
¶ Returns the ship body.
-------------------------------------
Getter Method
Signature
ShipBody
Returns: Return type: NXOpen.SelectBody
New in version NX5.0.0.
License requirements: None.
Waterline¶
-
MainDimensionsBuilder.
Waterline
¶ Returns the expression containing the position value of waterline along the Z axis.
-------------------------------------
Getter Method
Signature
Waterline
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
XMax¶
-
MainDimensionsBuilder.
XMax
¶ Returns the expression containing the x max value.
-------------------------------------
Getter Method
Signature
XMax
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
XMin¶
-
MainDimensionsBuilder.
XMin
¶ Returns the expression containing the x min value.
-------------------------------------
Getter Method
Signature
XMin
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
YMax¶
-
MainDimensionsBuilder.
YMax
¶ Returns the expression containing the y max value.
-------------------------------------
Getter Method
Signature
YMax
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ZMax¶
-
MainDimensionsBuilder.
ZMax
¶ Returns the expression containing the z max value.
-------------------------------------
Getter Method
Signature
ZMax
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ZMin¶
-
MainDimensionsBuilder.
ZMin
¶ Returns the expression containing the z min value.
-------------------------------------
Getter Method
Signature
ZMin
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
MainDimensionsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.