FeaturesToTagBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
FeaturesToTagBuilder
¶ Bases:
NXOpen.Builder
This class is used to add an attribute to profile features that have been modified by the user to display a ‘Metal to Metal’ design ‘feature’.
This attribute will be used later when the user switches from Ship Design mode to Ship Manufacturing mode… the Metal to Metal modifications will be suppressed.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateFeaturesToMarkBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
FeatureToTag | Returns the feature to tag. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ManageFeatureTag | Manages (set or unset) the ship manufacturing object on selected features |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FeatureToTag¶
-
FeaturesToTagBuilder.
FeatureToTag
¶ Returns the feature to tag.
-------------------------------------
Getter Method
Signature
FeatureToTag
Returns: Return type: NXOpen.Features.SelectFeatureList
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Method Detail¶
ManageFeatureTag¶
-
FeaturesToTagBuilder.
ManageFeatureTag
¶ Manages (set or unset) the ship manufacturing object on selected features
Signature
ManageFeatureTag(addMark, featureToMark)
Parameters: - addMark (bool) –
- featureToMark (
NXOpen.Features.Feature
) –
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Validate¶
-
FeaturesToTagBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.