EditBoundaryBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
EditBoundaryBuilder
¶ Bases:
NXOpen.Features.ShipDesign.ProfileSystemBuilder
Used to create a
NXOpen.Features.ShipDesign.EditBoundaryBuilder
which is used to change the boundaries and split knuckle locations of profile systems.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateEditBoundaryBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the tolerance, in degrees, used to determine when angles are zero. |
Boundary1 | Returns the collector containing the plate system, profile system, or datum plane that will be used to trim the first end of the generated profile system. |
Boundary1Plane | Returns or sets the defined plane that will be used to trim the first end of the generated profile system. |
Boundary2 | Returns the collector containing the plate system, profile system, or datum plane that will be used to trim the second end of the generated profile system. |
Boundary2Plane | Returns or sets the defined plane that will be used to trim the second end of the generated profile system. |
BoundaryReverse | Returns or sets the indication if the side of a single boundary should be changed to the other side or not. |
DistanceTolerance | Returns or sets the tolerance used to determine when distances are considered zero. |
FirstIntersectionPoints | Returns the selected intersection points between the curves and the first boundary. |
OrientationAngleRule | Returns or sets the angle rule to use when measuring angles. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProfileSystem | Returns the ship structures to change the boundary information |
ReversePathDirection | Returns or sets the flag that indicates if the default curve direction should be reversed or not. |
SecondIntersectionPoints | Returns the selected intersection points between the curves and the second boundary. |
SplitKnuckleLocations | Returns the collector containing the knuckle points that are to be used to create seams. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
UseNewDefaultSectionAlgorithm | Returns or sets the flag that indicates if the new default section algorithm is used. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreatePathCurves | Creates path curves for all the paths of the profile system. |
CreatePlaneForList | Create a NXOpen.Features.ShipDesign.PlaneListBuilder to add a defined plane to a list. |
DeleteLastPathCurves | Deletes the path curves returned from a call to GetLastPathCurves() . |
DeletePathCurves | Deletes the path curves created from a call to CreatePathCurves() . |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetLastPathCurves | Gets the path curves used by NXOpen.Features.ShipDesign.OrientationDefinitionBuilder . |
GetObject | Returns the object currently being edited by this builder. |
GetSelectedKnuckles | Outputs the knuckle points that have been selected in seams. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetBoundaryOnePoints | Sets the selected intersection points for the first boundary. |
SetBoundaryTwoPoints | Set the selected intersection points for the second boundary. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetRegionPoints | Sets the points that identify which regions of the curves will be used. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ProfileSystem¶
-
EditBoundaryBuilder.
ProfileSystem
¶ Returns the ship structures to change the boundary information
-------------------------------------
Getter Method
Signature
ProfileSystem
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX12.0.0.
License requirements: None.
Method Detail¶
GetSelectedKnuckles¶
-
EditBoundaryBuilder.
GetSelectedKnuckles
¶ Outputs the knuckle points that have been selected in seams.
Signature
GetSelectedKnuckles(profile)
Parameters: profile ( NXOpen.Curve
) –Returns: Knuckle points that have been selected in seams. Return type: list of NXOpen.Point
New in version NX12.0.0.
License requirements: None.
Validate¶
-
EditBoundaryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.