MultiBendBendPropertiesBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
MultiBendBendPropertiesBuilder
¶ Bases:
NXOpen.Features.SheetMetal.FeatureBendPropertiesBuilder
Represents a Sheetmetal Multi Bend properties builder class.
This builder is used to interrogate the properties of multiple bends in the list. To create a new instance of this class, use
NXOpen.Features.SheetMetal.MultiBendBendPropertiesListBuilder.CreateMultiBendBendProperties()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
BendOptions | Returns the Sheet Metal Bend Options |
Inset | Returns or sets the inset |
ParentPlane | Returns or sets the plane |
Plane | Returns or sets the plane |
SketchParentPlane | Returns or sets the option to set sketch plane as parent |
Tag | Returns the Tag for this object. |
Value | Returns the offset |
Methods¶
Method | Description |
---|---|
DeleteMultiBendBendProperties | Deletes a multi bend properties. |
GetApplicationContext | Get the application context. |
SetApplicationContext | Set the application context. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MultiBendBendPropertiesBuilderInsets Enumeration | This enum defines the material inset types |
Property Detail¶
Inset¶
-
MultiBendBendPropertiesBuilder.
Inset
¶ Returns or sets the inset
-------------------------------------
Getter Method
Signature
Inset
Returns: Return type: NXOpen.Features.SheetMetal.MultiBendBendPropertiesBuilderInsets
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Inset
Parameters: inset ( NXOpen.Features.SheetMetal.MultiBendBendPropertiesBuilderInsets
) –New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
ParentPlane¶
-
MultiBendBendPropertiesBuilder.
ParentPlane
¶ Returns or sets the plane
-------------------------------------
Getter Method
Signature
ParentPlane
Returns: Return type: NXOpen.Plane
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentPlane
Parameters: plane ( NXOpen.Plane
) –New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Plane¶
-
MultiBendBendPropertiesBuilder.
Plane
¶ Returns or sets the plane
-------------------------------------
Getter Method
Signature
Plane
Returns: Return type: NXOpen.Plane
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane
Parameters: plane ( NXOpen.Plane
) –New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SketchParentPlane¶
-
MultiBendBendPropertiesBuilder.
SketchParentPlane
¶ Returns or sets the option to set sketch plane as parent
-------------------------------------
Getter Method
Signature
SketchParentPlane
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SketchParentPlane
Parameters: isSketchPlaneParent (bool) – New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
DeleteMultiBendBendProperties¶
-
MultiBendBendPropertiesBuilder.
DeleteMultiBendBendProperties
¶ Deletes a multi bend properties.
Signature
DeleteMultiBendBendProperties()
New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Validate¶
-
MultiBendBendPropertiesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.