JoggleInputListItemBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
JoggleInputListItemBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Sheetmetal joggle input list item builder class.
This builder is used to interrogate the joggle inputitems in the list.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.JoggleBuilder.CreateJoggleInputListItem()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Depth | Returns the depth |
Faces | Returns the faces |
ReverseDirection | Returns or sets the reverse direction |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Depth¶
-
JoggleInputListItemBuilder.
Depth
¶ Returns the depth
-------------------------------------
Getter Method
Signature
Depth
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Faces¶
-
JoggleInputListItemBuilder.
Faces
¶ Returns the faces
-------------------------------------
Getter Method
Signature
Faces
Returns: Return type: NXOpen.ScCollector
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
ReverseDirection¶
-
JoggleInputListItemBuilder.
ReverseDirection
¶ Returns or sets the reverse direction
-------------------------------------
Getter Method
Signature
ReverseDirection
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection
Parameters: reverseDirection (bool) – New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Method Detail¶
Validate¶
-
JoggleInputListItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.