EdgeRipBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
EdgeRipBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Edge Rip feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateEdgeRipFeatureBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Section | Returns or sets the section used by Edge Rip |
Sketch | Returns or sets the Slave Sketch used by the Edge Rip, If one exists. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetRipEdges | Edges to rip |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetRipEdges | Edges to rip |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify whether the builder data is valid for creating a Edge Rip or not. |
Property Detail¶
Section¶
-
EdgeRipBuilder.
Section
¶ Returns or sets the section used by Edge Rip
-------------------------------------
Getter Method
Signature
Section
Returns: Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
Section
Parameters: section ( NXOpen.Section
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Sketch¶
-
EdgeRipBuilder.
Sketch
¶ Returns or sets the Slave Sketch used by the Edge Rip, If one exists.
-------------------------------------
Getter Method
Signature
Sketch
Returns: Return type: NXOpen.Features.SketchFeature
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
Sketch
Parameters: sketch ( NXOpen.Features.SketchFeature
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Method Detail¶
GetRipEdges¶
-
EdgeRipBuilder.
GetRipEdges
¶ Edges to rip
Signature
GetRipEdges()
Returns: Rip Edges Return type: list of NXOpen.Edge
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetRipEdges¶
-
EdgeRipBuilder.
SetRipEdges
¶ Edges to rip
Signature
SetRipEdges(ripEdges)
Parameters: ripEdges (list of NXOpen.Edge
) – Rip EdgesNew in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Validate¶
-
EdgeRipBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
EdgeRipBuilder.
ValidateBuilderData
¶ Verify whether the builder data is valid for creating a Edge Rip or not.
If the Builder data is valid, returned value shall be 0
Signature
ValidateBuilderData()
Returns: Data Validity Flag. Return type: int New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)