ConvertInputListItemBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
ConvertInputListItemBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Sheetmetal convert to sheet metal corner list item builder class.
This builder is used to interrogate the corner items in the list.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.ConvertToSheetmetalBuilder.CreateConvertInputListItem()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
CornerFaces | Returns the corner faces |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CornerFaces¶
-
ConvertInputListItemBuilder.
CornerFaces
¶ Returns the corner faces
-------------------------------------
Getter Method
Signature
CornerFaces
Returns: Return type: NXOpen.ScCollector
New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
Validate¶
-
ConvertInputListItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.