RuledBuilder Class¶
-
class
NXOpen.Features.
RuledBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.Ruled
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateRuledBuilder()
Default values.
Property Value AlignmentMethod.AlignType Parameter IsShapePreserved True New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AlignmentMethod | Returns the alignment method |
BodyPreference | Returns or sets the body type options |
FirstSection | Returns or sets the first section |
IsShapePreserved | Returns or sets the preserve shape flag. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PositionTolerance | Returns or sets the position tolerance |
SecondSection | Returns or sets the second section |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AlignmentMethod¶
-
RuledBuilder.
AlignmentMethod
¶ Returns the alignment method
-------------------------------------
Getter Method
Signature
AlignmentMethod
Returns: Return type: NXOpen.GeometricUtilities.AlignmentMethodBuilder
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
BodyPreference¶
-
RuledBuilder.
BodyPreference
¶ Returns or sets the body type options
-------------------------------------
Getter Method
Signature
BodyPreference
Returns: Return type: NXOpen.GeometricUtilities.FeatureOptions
New in version NX7.5.0.
License requirements: features_modeling (“FEATURES MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
BodyPreference
Parameters: featureOptions ( NXOpen.GeometricUtilities.FeatureOptions
) –New in version NX7.5.0.
License requirements: features_modeling (“FEATURES MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
FirstSection¶
-
RuledBuilder.
FirstSection
¶ Returns or sets the first section
-------------------------------------
Getter Method
Signature
FirstSection
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
FirstSection
Parameters: section ( NXOpen.Section
) –New in version NX7.5.0.
License requirements: features_modeling (“FEATURES MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
IsShapePreserved¶
-
RuledBuilder.
IsShapePreserved
¶ Returns or sets the preserve shape flag.
When preserve shape is used, the input curves will not be approximated in constructing the ruled surface. Only Parameter and By Points alignment options are allowed if preserve shape is used.
-------------------------------------
Getter Method
Signature
IsShapePreserved
Returns: Return type: bool New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
IsShapePreserved
Parameters: isShapePreserved (bool) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
PositionTolerance¶
-
RuledBuilder.
PositionTolerance
¶ Returns or sets the position tolerance
-------------------------------------
Getter Method
Signature
PositionTolerance
Returns: Return type: float New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
PositionTolerance
Parameters: positionTolerance (float) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
SecondSection¶
-
RuledBuilder.
SecondSection
¶ Returns or sets the second section
-------------------------------------
Getter Method
Signature
SecondSection
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
SecondSection
Parameters: section ( NXOpen.Section
) –New in version NX7.5.0.
License requirements: features_modeling (“FEATURES MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
Method Detail¶
Validate¶
-
RuledBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.