IsoparametricCurvesBuilder Class¶
-
class
NXOpen.Features.
IsoparametricCurvesBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.IsoparametricCurves
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateIsoparametricCurvesBuilder()
Default values.
Property Value Associative 1 IsSpacingEnabled 0 IsSwitchDirection 0 IsUEnabled 1 IsVEnabled 0 Number 5 Placement Uniform Spacing 25 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative state. |
ConstraintManager | Returns the constraint manager. |
Direction | Returns or sets the direction type |
IsSpacingEnabled | Returns or sets the is spacing enabled |
IsSwitchDirection | Returns or sets the is switch direction |
IsUEnabled | Returns or sets the is u enabled |
IsVEnabled | Returns or sets the is v enabled |
Number | Returns or sets the number of curves |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Placement | Returns or sets the placement type |
SelectObject | Returns the select object for faces |
Spacing | Returns or sets the spacing to use when spacing is enabled |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetActivePoints | Sets key points that are selected or will be moved |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
UpdateIsoparametricCurves | Sets key points that are selected or will be moved |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
IsoparametricCurvesBuilderDirectionTypes Enumeration | Curve direction options |
IsoparametricCurvesBuilderPlacementTypes Enumeration | Curve creation options |
Property Detail¶
Associative¶
-
IsoparametricCurvesBuilder.
Associative
¶ Returns or sets the associative state.
Disables feature creation when false
-------------------------------------
Getter Method
Signature
Associative
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative
Parameters: associative (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ConstraintManager¶
-
IsoparametricCurvesBuilder.
ConstraintManager
¶ Returns the constraint manager.
Allows definition of key points to be used to control curve creation.
-------------------------------------
Getter Method
Signature
ConstraintManager
Returns: Return type: NXOpen.Features.GeometricConstraintDataManager
New in version NX8.0.0.
License requirements: None.
Direction¶
-
IsoparametricCurvesBuilder.
Direction
¶ Returns or sets the direction type
-------------------------------------
Getter Method
Signature
Direction
Returns: Return type: NXOpen.Features.IsoparametricCurvesBuilderDirectionTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction
Parameters: direction ( NXOpen.Features.IsoparametricCurvesBuilderDirectionTypes
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsSpacingEnabled¶
-
IsoparametricCurvesBuilder.
IsSpacingEnabled
¶ Returns or sets the is spacing enabled
-------------------------------------
Getter Method
Signature
IsSpacingEnabled
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSpacingEnabled
Parameters: isSpacingEnabled (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsSwitchDirection¶
-
IsoparametricCurvesBuilder.
IsSwitchDirection
¶ Returns or sets the is switch direction
-------------------------------------
Getter Method
Signature
IsSwitchDirection
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSwitchDirection
Parameters: isSwitchDirection (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsUEnabled¶
-
IsoparametricCurvesBuilder.
IsUEnabled
¶ Returns or sets the is u enabled
-------------------------------------
Getter Method
Signature
IsUEnabled
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsUEnabled
Parameters: isUEnabled (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsVEnabled¶
-
IsoparametricCurvesBuilder.
IsVEnabled
¶ Returns or sets the is v enabled
-------------------------------------
Getter Method
Signature
IsVEnabled
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsVEnabled
Parameters: isVEnabled (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Number¶
-
IsoparametricCurvesBuilder.
Number
¶ Returns or sets the number of curves
-------------------------------------
Getter Method
Signature
Number
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Number
Parameters: number (int) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Placement¶
-
IsoparametricCurvesBuilder.
Placement
¶ Returns or sets the placement type
-------------------------------------
Getter Method
Signature
Placement
Returns: Return type: NXOpen.Features.IsoparametricCurvesBuilderPlacementTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Placement
Parameters: placement ( NXOpen.Features.IsoparametricCurvesBuilderPlacementTypes
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SelectObject¶
-
IsoparametricCurvesBuilder.
SelectObject
¶ Returns the select object for faces
-------------------------------------
Getter Method
Signature
SelectObject
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.0.0.
License requirements: None.
Spacing¶
-
IsoparametricCurvesBuilder.
Spacing
¶ Returns or sets the spacing to use when spacing is enabled
-------------------------------------
Getter Method
Signature
Spacing
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Spacing
Parameters: spacing (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
SetActivePoints¶
-
IsoparametricCurvesBuilder.
SetActivePoints
¶ Sets key points that are selected or will be moved
Signature
SetActivePoints(points, masterPoint)
Parameters: - points (list of
NXOpen.Point
) – Key points - masterPoint (
NXOpen.Point
) – Point which user actually moves to move a group of selected points
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- points (list of
UpdateIsoparametricCurves¶
-
IsoparametricCurvesBuilder.
UpdateIsoparametricCurves
¶ Sets key points that are selected or will be moved
Signature
UpdateIsoparametricCurves()
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
IsoparametricCurvesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.