GeodesicChamferBuilder Class¶
-
class
NXOpen.Features.
GeodesicChamferBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.GeodesicChamfer
builder for GeodesicChamfer command.To create a new instance of this class, use
NXOpen.Features.GeodesicSketchCollection.CreateGeodesicChamferBuilder()
Default values.
Property Value Distance.Value 10 (millimeters part), 0.5 (inches part) New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Distance | Returns the distance |
FirstCurve | Returns or sets the first selected curve in the section |
FirstPoint | Returns or sets the first selection point |
FirstSection | Returns or sets the first section of curves to chamfer |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SecondCurve | Returns or sets the second selected curve in the section |
SecondPoint | Returns or sets the second selection point |
SecondSection | Returns or sets the second section of curves to chamfer |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Distance¶
-
GeodesicChamferBuilder.
Distance
¶ Returns the distance
-------------------------------------
Getter Method
Signature
Distance
Returns: Distance NXOpen.Expression
Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
FirstCurve¶
-
GeodesicChamferBuilder.
FirstCurve
¶ Returns or sets the first selected curve in the section
-------------------------------------
Getter Method
Signature
FirstCurve
Returns: NXOpen.Curve
Return type: NXOpen.Curve
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstCurve
Parameters: firstCurve ( NXOpen.Curve
) –NXOpen.Curve
New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FirstPoint¶
-
GeodesicChamferBuilder.
FirstPoint
¶ Returns or sets the first selection point
-------------------------------------
Getter Method
Signature
FirstPoint
Returns: First Point Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstPoint
Parameters: firstPoint (float) – First Point New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FirstSection¶
-
GeodesicChamferBuilder.
FirstSection
¶ Returns or sets the first section of curves to chamfer
-------------------------------------
Getter Method
Signature
FirstSection
Returns: NXOpen.Section
Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstSection
Parameters: firstSection ( NXOpen.Section
) –NXOpen.Section
New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondCurve¶
-
GeodesicChamferBuilder.
SecondCurve
¶ Returns or sets the second selected curve in the section
-------------------------------------
Getter Method
Signature
SecondCurve
Returns: NXOpen.Curve
Return type: NXOpen.Curve
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondCurve
Parameters: secondCurve ( NXOpen.Curve
) –NXOpen.Curve
New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondPoint¶
-
GeodesicChamferBuilder.
SecondPoint
¶ Returns or sets the second selection point
-------------------------------------
Getter Method
Signature
SecondPoint
Returns: Second Point Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondPoint
Parameters: secondPoint (float) – Second Point New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondSection¶
-
GeodesicChamferBuilder.
SecondSection
¶ Returns or sets the second section of curves to chamfer
-------------------------------------
Getter Method
Signature
SecondSection
Returns: NXOpen.Section
Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondSection
Parameters: secondSection ( NXOpen.Section
) –NXOpen.Section
New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
GeodesicChamferBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.