EmbossBuilder Class¶
-
class
NXOpen.Features.
EmbossBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents an emboss feature builder that creates or edits an emboss feature.
This class provides methods to set and get the multiple region subobjects and tolerance.
The following is default value:
**Tolerance</b> Distance tolerance 0.001/0.0254[in/mm]
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateEmbossBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the distance tolerance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetRegions | The emboss regions |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
MakeParentSketchInternal | Set the parent sketch internalization status for use during emboss feature creation |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetRegions | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Tolerance¶
-
EmbossBuilder.
Tolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
Tolerance
Returns: distance tolerance Return type: float New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tolerance (float) – distance tolerance New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
GetRegions¶
-
EmbossBuilder.
GetRegions
¶ The emboss regions
Signature
GetRegions()
Returns: Array of emboss region objects. In NX4, only one region is supported. Return type: list of NXOpen.Features.EmbossRegion
New in version NX4.0.0.
License requirements: None.
MakeParentSketchInternal¶
-
EmbossBuilder.
MakeParentSketchInternal
¶ Set the parent sketch internalization status for use during emboss feature creation
Signature
MakeParentSketchInternal(internalizeParentSketch)
Parameters: internalizeParentSketch (bool) – If true, internalize the parent sketch, else the sketch will remain external. New in version NX4.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetRegions¶
-
EmbossBuilder.
SetRegions
¶ Signature
SetRegions(regions)
Parameters: regions (list of NXOpen.Features.EmbossRegion
) – Array of emboss region objects. In NX4, only one region is supported.New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
EmbossBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.