EmbeddedOperationBuilder Class

class NXOpen.Features.EmbeddedOperationBuilder

Bases: NXOpen.Builder

Represents an EmbeddedOperationBuilder

This is an abstract class, and cannot be instantiated.

New in version NX5.0.0.

Properties

Property Description
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
CommitOperation Commits the operation and creates the feature.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
GetOperation Returns the feature currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Method Detail

CommitOperation

EmbeddedOperationBuilder.CommitOperation

Commits the operation and creates the feature.

If it’s for a recipe curve of Drafting sketch, there will be no feature returned because Drafting sketch is featureless.

Signature CommitOperation()

Returns:
Return type:NXOpen.Features.Feature

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

GetOperation

EmbeddedOperationBuilder.GetOperation

Returns the feature currently being edited by this builder.

If a new feature is being created, and the builder has not yet been commited, returns None.

Signature GetOperation()

Returns:
Return type:NXOpen.Features.Feature

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

Validate

EmbeddedOperationBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.