CutFaceBuilder Class¶
-
class
NXOpen.Features.
CutFaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder for a cut face feature.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateCutFaceBuilder()
Default values.
Property Value FaceToCut.CoaxialEnabled 0 FaceToCut.CoplanarAxesEnabled 0 FaceToCut.CoplanarEnabled 0 FaceToCut.EqualDiameterEnabled 0 FaceToCut.OffsetEnabled 0 FaceToCut.ParallelEnabled 0 FaceToCut.PerpendicularEnabled 0 FaceToCut.SymmetricEnabled 0 FaceToCut.TangentEnabled 0 FaceToCut.ThicknessChainEnabled 0 FaceToCut.UseFaceBrowse 1 Motion.DeltaEnum ReferenceWcsWorkPart Motion.DeltaXc.Value 0.0 Motion.DeltaYc.Value 0.0 Motion.DeltaZc.Value 0.0 Motion.Option DistanceAngle New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DoPaste | Returns or sets the do paste option defines whether paste the cut faces to a target body. |
FaceToCut | Returns the face recognition builder holding the faces to cut. |
Motion | Returns the motion about which the cut faces move |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReverseDirection | Returns or sets the reverse direction. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetBody | Returns the target body. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DoPaste¶
-
CutFaceBuilder.
DoPaste
¶ Returns or sets the do paste option defines whether paste the cut faces to a target body.
-------------------------------------
Getter Method
Signature
DoPaste
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoPaste
Parameters: doPaste (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
FaceToCut¶
-
CutFaceBuilder.
FaceToCut
¶ Returns the face recognition builder holding the faces to cut.
-------------------------------------
Getter Method
Signature
FaceToCut
Returns: Return type: NXOpen.Features.FaceRecognitionBuilder
New in version NX6.0.0.
License requirements: None.
Motion¶
-
CutFaceBuilder.
Motion
¶ Returns the motion about which the cut faces move
-------------------------------------
Getter Method
Signature
Motion
Returns: Return type: NXOpen.GeometricUtilities.ModlMotion
New in version NX6.0.0.
License requirements: None.
ReverseDirection¶
-
CutFaceBuilder.
ReverseDirection
¶ Returns or sets the reverse direction.
A flag to indicate whether the target body direction is reversed, disabled if target body is solid.
-------------------------------------
Getter Method
Signature
ReverseDirection
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection
Parameters: reverseDirection (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
TargetBody¶
-
CutFaceBuilder.
TargetBody
¶ Returns the target body.
The target body can be a solid or sheet.
-------------------------------------
Getter Method
Signature
TargetBody
Returns: Return type: NXOpen.SelectBody
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CutFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.