CustomFeaturePostUpdateEvent Class¶
-
class
NXOpen.Features.
CustomFeaturePostUpdateEvent
¶ Bases:
NXOpen.Features.CustomFeatureEvent
Represents the event data for post-update callback for custom feature.
This class cannot be created
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ErrorCode | Returns or sets the error occured during the event |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateOutputFeatureData | Create output feature data |
GetConstructionFeatures | The custom feature get construction features |
GetCustomFeature | Get the custom feature of the event |
GetNXObject | Returns the Solid body |
GetOutputFeatures | The output features created in post update event |
GetParasolidId | Get the Parasolid tag of Solid body |
SetOutputFeatures | The output features created in post update event |
Method Detail¶
CreateOutputFeatureData¶
-
CustomFeaturePostUpdateEvent.
CreateOutputFeatureData
¶ Create output feature data
Signature
CreateOutputFeatureData(feature)
Parameters: feature ( NXOpen.Features.Feature
) – The feature for which the data object is to be createdReturns: The object of OutputFeatureData Return type: NXOpen.Features.OutputFeatureData
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetOutputFeatures¶
-
CustomFeaturePostUpdateEvent.
SetOutputFeatures
¶ The output features created in post update event
Signature
SetOutputFeatures(outputFeatureData)
Parameters: outputFeatureData (list of NXOpen.Features.OutputFeatureData
) – Input array of NXOpen FeaturesNew in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)