AssemblyCutBuilder Class¶
-
class
NXOpen.Features.
AssemblyCutBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.AssemblyCut
builder.Input to this class can be PSM facet objects.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateAssemblyCutBuilder()
Default values.
Property Value HideToolBodyFlag 1 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ContextComponent | Returns or sets the context component for the assembly cut operation |
HideToolBodyFlag | Returns or sets the hide tool body flag |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetBody | Returns the target body |
ToolBody | Returns the tool body |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetOperationFailures | Gets the list of errors encountered in the Assembly cut operation. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ContextComponent¶
-
AssemblyCutBuilder.
ContextComponent
¶ Returns or sets the context component for the assembly cut operation
-------------------------------------
Getter Method
Signature
ContextComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContextComponent
Parameters: workOccTag ( NXOpen.Assemblies.Component
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
HideToolBodyFlag¶
-
AssemblyCutBuilder.
HideToolBodyFlag
¶ Returns or sets the hide tool body flag
-------------------------------------
Getter Method
Signature
HideToolBodyFlag
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HideToolBodyFlag
Parameters: hideToolBodyFlag (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TargetBody¶
-
AssemblyCutBuilder.
TargetBody
¶ Returns the target body
-------------------------------------
Getter Method
Signature
TargetBody
Returns: Target body Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
ToolBody¶
-
AssemblyCutBuilder.
ToolBody
¶ Returns the tool body
-------------------------------------
Getter Method
Signature
ToolBody
Returns: Tool body Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
GetOperationFailures¶
-
AssemblyCutBuilder.
GetOperationFailures
¶ Gets the list of errors encountered in the Assembly cut operation.
Caller needs to dispose the error list after processing it.
Signature
GetOperationFailures()
Returns: Return type: NXOpen.ErrorList
New in version NX10.0.0.
License requirements: None.
Validate¶
-
AssemblyCutBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.