RemoveUndercutsBuilder Class¶
-
class
NXOpen.Facet.
RemoveUndercutsBuilder
¶ Bases:
NXOpen.Builder
This class handles the removal of undercut regions of a facet body.
To create a new instance of this class, use
NXOpen.Facet.FacetModelingCollection.CreateRemoveUndercutsBuilder()
Default values.
Property Value DraftAngle.Value 0 IsEditCopy 0 New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
DraftAngle | Returns the draft angle |
DrawDirection | Returns or sets the draft vector |
FacetBody | Returns the facet body. |
IsEditCopy | Returns or sets the flag indicating if the fixing undercuts is on the copy of the input facet body. |
MatchFace | Returns or sets the match tangent to face. |
PartingObject | Returns the parting object |
SelectedCurve | Returns the selected isocline curve. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GenerateIsoclines | The generation of isoclines. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DraftAngle¶
-
RemoveUndercutsBuilder.
DraftAngle
¶ Returns the draft angle
-------------------------------------
Getter Method
Signature
DraftAngle
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
DrawDirection¶
-
RemoveUndercutsBuilder.
DrawDirection
¶ Returns or sets the draft vector
-------------------------------------
Getter Method
Signature
DrawDirection
Returns: Return type: NXOpen.Direction
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawDirection
Parameters: drawDirection ( NXOpen.Direction
) –New in version NX12.0.0.
License requirements: None.
FacetBody¶
-
RemoveUndercutsBuilder.
FacetBody
¶ Returns the facet body.
Inputs to this command can be convergent objects
-------------------------------------
Getter Method
Signature
FacetBody
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX12.0.0.
License requirements: None.
IsEditCopy¶
-
RemoveUndercutsBuilder.
IsEditCopy
¶ Returns or sets the flag indicating if the fixing undercuts is on the copy of the input facet body.
-------------------------------------
Getter Method
Signature
IsEditCopy
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsEditCopy
Parameters: isEditCopy (bool) – New in version NX12.0.0.
License requirements: nx_polygon_modeling (” NX Polygon Modeling”)
MatchFace¶
-
RemoveUndercutsBuilder.
MatchFace
¶ Returns or sets the match tangent to face.
Math the shorter face by bridging the input face to the edge of the longer face at the parting objet.
-------------------------------------
Getter Method
Signature
MatchFace
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MatchFace
Parameters: matchFace (bool) – New in version NX12.0.0.
License requirements: nx_polygon_modeling (” NX Polygon Modeling”)
PartingObject¶
-
RemoveUndercutsBuilder.
PartingObject
¶ Returns the parting object
-------------------------------------
Getter Method
Signature
PartingObject
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX12.0.0.
License requirements: None.
SelectedCurve¶
-
RemoveUndercutsBuilder.
SelectedCurve
¶ Returns the selected isocline curve.
The undercut related to the selected isocline curve will be removed.
-------------------------------------
Getter Method
Signature
SelectedCurve
Returns: Return type: NXOpen.ScCollector
New in version NX12.0.0.
License requirements: None.
Method Detail¶
GenerateIsoclines¶
-
RemoveUndercutsBuilder.
GenerateIsoclines
¶ The generation of isoclines.
Create isocline curves on the input facet body.
Signature
GenerateIsoclines()
New in version NX12.0.0.
License requirements: nx_polygon_modeling (” NX Polygon Modeling”)
Validate¶
-
RemoveUndercutsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.