MergeFacetFacesBuilder Class¶
-
class
NXOpen.Facet.
MergeFacetFacesBuilder
¶ Bases:
NXOpen.Builder
Represents a
Facet.MergeFacetFacesBuilder
builderTo create a new instance of this class, use
NXOpen.Facet.FacetModelingCollection.CreateMergeFacetFacesBuilder()
Default values.
Property Value IsEditCopy 0 New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
FaceCollector | Returns the face collector |
IsEditCopy | Returns or sets the value indicating if a copy of the facet body to be used for Merge facet faces without altering the original |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FaceCollector¶
-
MergeFacetFacesBuilder.
FaceCollector
¶ Returns the face collector
-------------------------------------
Getter Method
Signature
FaceCollector
Returns: Return type: NXOpen.ScCollector
New in version NX12.0.0.
License requirements: None.
IsEditCopy¶
-
MergeFacetFacesBuilder.
IsEditCopy
¶ Returns or sets the value indicating if a copy of the facet body to be used for Merge facet faces without altering the original
-------------------------------------
Getter Method
Signature
IsEditCopy
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsEditCopy
Parameters: isEditCopy (bool) – New in version NX12.0.0.
License requirements: nx_polygon_modeling (” NX Polygon Modeling”)
Method Detail¶
Validate¶
-
MergeFacetFacesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.