FacetedEdge Class¶
-
class
NXOpen.Facet.
FacetedEdge
¶ Bases:
NXOpen.DisplayableObject
,NXOpen.IBaseCurve
Represents a faceted edge.
Instances of this class may be generated when recording a journal, but they cannot be created directly.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
EdgeType | Returns the type of the facet edge |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsReference | Returns the reference state of a curve |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBody | Returns the body containing this edge |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetCurveData | Returns the curve information for the facet edge Parameter description faceted_edge : The input edge tag for which curve information is required. |
GetFaces | Returns the faces connected to the edge |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLength | Returns the length of the object |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetVertices | Returns the vertices of the edge. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Enumerations¶
FacetedEdgeFacetededgeType Enumeration | Facet Edge type |
Property Detail¶
EdgeType¶
-
FacetedEdge.
EdgeType
¶ Returns the type of the facet edge
-------------------------------------
Getter Method
Signature
EdgeType
Returns: Return type: NXOpen.Facet.FacetedEdgeFacetededgeType
New in version NX8.5.1.
License requirements: None.
IsOccurrence¶
-
FacetedEdge.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
IsReference¶
-
FacetedEdge.
IsReference
¶ Returns the reference state of a curve
-------------------------------------
Getter Method
Signature
IsReference
Returns: True - Reference; False - Not Reference Return type: bool New in version NX8.0.0.
License requirements: None.
JournalIdentifier¶
-
FacetedEdge.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
FacetedEdge.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
FacetedEdge.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FacetedEdge.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
FacetedEdge.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
FacetedEdge.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetBody¶
-
FacetedEdge.
GetBody
¶ Returns the body containing this edge
Signature
GetBody()
Returns: Return type: NXOpen.Facet.FacetedBody
New in version NX8.5.1.
License requirements: None.
GetCurveData¶
-
FacetedEdge.
GetCurveData
¶ Returns the curve information for the facet edge
Parameter description faceted_edge : The input edge tag for which curve information is required. PNT3_p_t position : Line: Position on Line Circle/Ellipse: Center Point Spline/Intersection-Curve: Start Point of Curve. PNT3_p_t dir_or_end_pt : Line : Direction of the Line Circle: Normal to Plane Axis. Ellipse: Major Axis Spline/Intersection-Curve: End Point. PNT3_p_t x_axis : Circle: Axis from Center to Start Point, Ellipse: Minor Axis Not valid for other types.
double* radius : Circle: Radius Ellipse: Major Radius Not valid for other types.
double* minor_radius : Ellipse: Minor Radius Not valid for other types.
Signature
GetCurveData()
Returns: a tuple Return type: A tuple consisting of (position, dirOrEndPt, xAxis, radius, minorRadius). position is a NXOpen.Point3d
. dirOrEndPt is aNXOpen.Point3d
. xAxis is aNXOpen.Point3d
. radius is a float. minorRadius is a float.New in version NX8.5.1.
License requirements: None.
GetFaces¶
-
FacetedEdge.
GetFaces
¶ Returns the faces connected to the edge
Signature
GetFaces()
Returns: Return type: list of NXOpen.Facet.FacetedFace
New in version NX8.5.1.
License requirements: None.
GetLength¶
-
FacetedEdge.
GetLength
¶ Returns the length of the object
Signature
GetLength()
Returns: Return type: float New in version NX3.0.0.
License requirements: None.
GetVertices¶
-
FacetedEdge.
GetVertices
¶ Returns the vertices of the edge.
If the edge is closed, the second vertex is the same as the first.
Signature
GetVertices()
Returns: a tuple Return type: A tuple consisting of (vertex1, vertex2). vertex1 is a NXOpen.Point3d
. First vertex in the edge vertex2 is aNXOpen.Point3d
. Second vertex in the edgeNew in version NX8.5.1.
License requirements: None.
Print¶
-
FacetedEdge.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
FacetedEdge.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.