FaceRibFacesRule Class¶
-
class
NXOpen.
FaceRibFacesRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects all rib faces.New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the rib faces rule: NXOpen.FaceRibFacesRule |
GetDefiningData | Gets the data for the rib faces rule: NXOpen.FaceRibFacesRule |
Method Detail¶
Dispose¶
-
FaceRibFacesRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.
GetData¶
-
FaceRibFacesRule.
GetData
¶ Gets the data for the rib faces rule:
NXOpen.FaceRibFacesRule
Signature
GetData()
Returns: Faces which creates this rule Return type: NXOpen.Face
New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
GetDefiningData¶
-
FaceRibFacesRule.
GetDefiningData
¶ Gets the data for the rib faces rule:
NXOpen.FaceRibFacesRule
Signature
GetDefiningData()
Returns: a tuple Return type: A tuple consisting of (face, includeBoundaryBlends, travserseInteriorLoops) face is a
NXOpen.Face
. Faces which creates this ruleincludeBoundaryBlends is a bool. true if the rule is not to identify any blends at the boundary travserseInteriorLoops is a bool. true if interrior loops are to be processed. .. versionadded:: NX6.0.0License requirements: gateway (“UG GATEWAY”)