FaceRegionRule Class¶
-
class
NXOpen.
FaceRegionRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects a region of faces.New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the face region rule: NXOpen.FaceRegionRule |
Method Detail¶
Dispose¶
-
FaceRegionRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetData¶
-
FaceRegionRule.
GetData
¶ Gets the data for the face region rule:
NXOpen.FaceRegionRule
Signature
GetData()
Returns: Boundary Faces which creates this rule Return type: list of NXOpen.Face
New in version NX4.0.0.
Deprecated since version NX8.0.0: This functionality is no longer supported.
License requirements: gateway (“UG GATEWAY”)