Ellipse Class¶
-
class
NXOpen.
Ellipse
¶ Bases:
NXOpen.Conic
Represents an ellipse curve.
The start and end angles are measured relative to the X and Y axes of the orientation matrix of the conic. To create a new instance of this class, use
NXOpen.CurveCollection.CreateEllipse()
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
CenterPoint | Returns the center. |
Color | Returns or sets the color of the object. |
EndAngle | Returns the end angle. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsReference | Returns the reference state of a curve |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
MajorRadius | Returns the major radius. |
Matrix | Returns the orientation matrix. |
MinorRadius | Returns the minor radius. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
RotationAngle | Returns the rotation angle. |
StartAngle | Returns the start angle. |
Tag | Returns the Tag for this object. |
Update | Returns the update option. |
Visibility | Returns the visibility. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Evaluate | Evaluate a smart object. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDraftingCurveInfo | Creates new DraftingCurveInfo object |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLength | Returns the length of the object |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetOrientation | Gets the orientation of the conic. |
GetParameters | Gets the parameters of the ellipse - the major/minor radii, start/end angles and the centre of the ellipse. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
ProtectFromDelete | Protects the SmartObject from being deleted if any referencing objects are deleted. |
RedisplayObject | Redisplays the object in all views. |
ReleaseDeleteProtection | Removes delete protection from the SmartObject. |
RemoveParameters | Removes the smart object parameters. |
RemoveViewDependency | Remove dependency on all views from an object. |
ReplaceParameters | Edit a smart object by replacing its parameters using parameters of other smart object of the same class. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetOrientation | Sets the center of the conic. |
SetParameters | Sets the parameters of the ellipse - the major/minor radii, start/end angles and the centre of the ellipse. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetVisibility | Sets the visibility. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Property Detail¶
EndAngle¶
-
Ellipse.
EndAngle
¶ Returns the end angle.
-------------------------------------
Getter Method
Signature
EndAngle
Returns: In radians Return type: float New in version NX3.0.0.
License requirements: None.
IsOccurrence¶
-
Ellipse.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
IsReference¶
-
Ellipse.
IsReference
¶ Returns the reference state of a curve
-------------------------------------
Getter Method
Signature
IsReference
Returns: True - Reference; False - Not Reference Return type: bool New in version NX8.0.0.
License requirements: None.
JournalIdentifier¶
-
Ellipse.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
MajorRadius¶
-
Ellipse.
MajorRadius
¶ Returns the major radius.
-------------------------------------
Getter Method
Signature
MajorRadius
Returns: Return type: float New in version NX3.0.0.
License requirements: None.
MinorRadius¶
-
Ellipse.
MinorRadius
¶ Returns the minor radius.
-------------------------------------
Getter Method
Signature
MinorRadius
Returns: Return type: float New in version NX3.0.0.
License requirements: None.
Name¶
-
Ellipse.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Ellipse.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Ellipse.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Ellipse.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
Ellipse.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetDraftingCurveInfo¶
-
Ellipse.
GetDraftingCurveInfo
¶ Creates new DraftingCurveInfo object
Signature
GetDraftingCurveInfo()
Returns: New DraftingCurveInfo object. Returns None if the input curve is not a drafting curve :rtype:
NXOpen.Drawings.DraftingCurveInfo
New in version NX10.0.0.
License requirements: None.
GetLength¶
-
Ellipse.
GetLength
¶ Returns the length of the object
Signature
GetLength()
Returns: Return type: float New in version NX3.0.0.
License requirements: None.
GetParameters¶
-
Ellipse.
GetParameters
¶ Gets the parameters of the ellipse - the major/minor radii, start/end angles and the centre of the ellipse.
Signature
GetParameters()
Returns: a tuple Return type: A tuple consisting of (majorRadius, minorRadius, startAngle, endAngle, rotationAngle, center). majorRadius is a float. minorRadius is a float. startAngle is a float. In radians endAngle is a float. In radians rotationAngle is a float. In radians center is a NXOpen.Point3d
.New in version NX11.0.0.
License requirements: None.
Print¶
-
Ellipse.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
Ellipse.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetParameters¶
-
Ellipse.
SetParameters
¶ Overloaded method SetParameters
SetParameters(majorRadius, minorRadius, startAngle, endAngle, rotationAngle, center)
SetParameters(startPoint, endPoint, anchorPoint, rho)
-------------------------------------
Sets the parameters of the ellipse - the major/minor radii, start/end angles and the centre of the ellipse.
Signature
SetParameters(majorRadius, minorRadius, startAngle, endAngle, rotationAngle, center)
Parameters: - majorRadius (float) –
- minorRadius (float) –
- startAngle (float) – In radians
- endAngle (float) – In radians
- rotationAngle (float) – In radians
- center (
NXOpen.Point3d
) –
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Sets the start, end, anchor, rho of the conic.
Signature
SetParameters(startPoint, endPoint, anchorPoint, rho)
Parameters: - startPoint (
NXOpen.Point3d
) – - endPoint (
NXOpen.Point3d
) – - anchorPoint (
NXOpen.Point3d
) – - rho (float) –
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------