ViewWorkflowBuilder Class¶
-
class
NXOpen.Drawings.
ViewWorkflowBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Drawings.ViewWorkflowBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ActiveSketchViewColor | Returns or sets the active views border color |
AssociativeAlignment | Returns or sets the associative alignment enable alignement between views |
BorderColor | Returns or sets the border color of view |
CursorTracking | Returns or sets the cursor tracking enable XC/YC coordinates in dynamic input boxes when placing a view on a drawing |
DisplayBorders | Returns or sets the display view borders on the the drawing |
EnableSmoothEdgesForLWView | Returns or sets the setting is not needed anymore because the smooth edges are correctly supported now for smart lightweight views. |
FaceDisplay | Returns or sets the face display provides options in an extracted edge view that are available for selection |
HandlingBodies | Returns or sets the handling bodies provides option for update view without lightweight data |
HandlingBodiesTypes | Returns or sets the handling bodies provides option for update view without lightweight data |
LargeAssemblyStepThreshold | Returns or sets the large assembly step threshold option establishes the minimum number of components (loaded or unloaded) a part may have to be considered a large assembly. |
LoadComponentsOnDemand | Returns or sets whether or not to load the components on demand for smart lightweight views |
OnLegacyViewUpdate | Returns or sets the on legacy view update determines whether or not components should be loaded as needed to update lightweight views |
OnViewSelection | Returns or sets the on view selection determines whether or not components should be loaded as needed for selection in lightweight views for accurate dimensioning |
PreviewStyle | Returns or sets the style of the preview when adding a view to the drawing |
SelectGeometryProjectedAsArcs | Returns or sets the Select Geometry Projected as Arcs provides options for selection of SPLARCs entity for centerlines and Annotations |
ShowFacetEdges | Returns or sets the show facet edges determines whether or not facet edges will be shown on shaded faces when displaying a drawing sheet |
Tag | Returns the Tag for this object. |
UseLineAntialiasing | Returns or sets the use line antialiasing |
UseTranslucency | Returns or sets the use translucency determines translucency settings for faces when displaying a drawing sheet |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ViewWorkflowBuilderDisplay Enumeration | Represents the extracted edge face display option |
ViewWorkflowBuilderHandlingBodiesType Enumeration | Represents option for handling bodies with no valid lightweight data |
ViewWorkflowBuilderHandlingbodies Enumeration | Represents option for handling bodies with no valid lightweight data |
ViewWorkflowBuilderSplarcs Enumeration | Represents the setting for splarcs geometry projected as arc option |
ViewWorkflowBuilderStyle Enumeration | Represents the preview stle option |
Property Detail¶
ActiveSketchViewColor¶
-
ViewWorkflowBuilder.
ActiveSketchViewColor
¶ Returns or sets the active views border color
-------------------------------------
Getter Method
Signature
ActiveSketchViewColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveSketchViewColor
Parameters: activeSketchViewColor (Id) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
AssociativeAlignment¶
-
ViewWorkflowBuilder.
AssociativeAlignment
¶ Returns or sets the associative alignment enable alignement between views
-------------------------------------
Getter Method
Signature
AssociativeAlignment
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssociativeAlignment
Parameters: associativeAlignment (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
BorderColor¶
-
ViewWorkflowBuilder.
BorderColor
¶ Returns or sets the border color of view
-------------------------------------
Getter Method
Signature
BorderColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BorderColor
Parameters: borderColor (Id) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
CursorTracking¶
-
ViewWorkflowBuilder.
CursorTracking
¶ Returns or sets the cursor tracking enable XC/YC coordinates in dynamic input boxes when placing a view on a drawing
-------------------------------------
Getter Method
Signature
CursorTracking
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CursorTracking
Parameters: cursorTracking (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
DisplayBorders¶
-
ViewWorkflowBuilder.
DisplayBorders
¶ Returns or sets the display view borders on the the drawing
-------------------------------------
Getter Method
Signature
DisplayBorders
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayBorders
Parameters: displayBorders (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
EnableSmoothEdgesForLWView¶
-
ViewWorkflowBuilder.
EnableSmoothEdgesForLWView
¶ Returns or sets the setting is not needed anymore because the smooth edges are correctly supported now for smart lightweight views.
We recommend removing this call from existing programs.
-------------------------------------
Getter Method
Signature
EnableSmoothEdgesForLWView
Returns: Return type: bool New in version NX9.0.0.
Deprecated since version NX11.0.0: Replacement is not needed. We recommend removing this call from existing programs.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnableSmoothEdgesForLWView
Parameters: enableSmoothEdgesForLWView (bool) – New in version NX9.0.0.
Deprecated since version NX11.0.0: Replacement is not needed. We recommend removing this call from existing programs.
License requirements: drafting (“DRAFTING”)
FaceDisplay¶
-
ViewWorkflowBuilder.
FaceDisplay
¶ Returns or sets the face display provides options in an extracted edge view that are available for selection
-------------------------------------
Getter Method
Signature
FaceDisplay
Returns: Return type: NXOpen.Drawings.ViewWorkflowBuilderDisplay
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceDisplay
Parameters: faceDisplay ( NXOpen.Drawings.ViewWorkflowBuilderDisplay
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
HandlingBodies¶
-
ViewWorkflowBuilder.
HandlingBodies
¶ Returns or sets the handling bodies provides option for update view without lightweight data
-------------------------------------
Getter Method
Signature
HandlingBodies
Returns: Return type: NXOpen.Drawings.ViewWorkflowBuilderHandlingbodies
New in version NX9.0.0.
Deprecated since version NX9.0.3: Use
NXOpen.Drawings.ViewWorkflowBuilder.HandlingBodiesTypes()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
HandlingBodies
Parameters: handlingBodies ( NXOpen.Drawings.ViewWorkflowBuilderHandlingbodies
) –New in version NX9.0.0.
Deprecated since version NX9.0.3: Use
NXOpen.Drawings.ViewWorkflowBuilder.HandlingBodiesTypes()
instead.License requirements: drafting (“DRAFTING”)
HandlingBodiesTypes¶
-
ViewWorkflowBuilder.
HandlingBodiesTypes
¶ Returns or sets the handling bodies provides option for update view without lightweight data
-------------------------------------
Getter Method
Signature
HandlingBodiesTypes
Returns: Return type: NXOpen.Drawings.ViewWorkflowBuilderHandlingBodiesType
New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
HandlingBodiesTypes
Parameters: handlingBodiesTypes ( NXOpen.Drawings.ViewWorkflowBuilderHandlingBodiesType
) –New in version NX9.0.3.
License requirements: None.
LargeAssemblyStepThreshold¶
-
ViewWorkflowBuilder.
LargeAssemblyStepThreshold
¶ Returns or sets the large assembly step threshold option establishes the minimum number of components (loaded or unloaded) a part may have to be considered a large assembly.
When the number of components exceeds this number, the View Creation Wizard provides an extra step to optimize part settings for large assemblies. A value of zero will force the system to always use the optimized part settings for large assemblies
-------------------------------------
Getter Method
Signature
LargeAssemblyStepThreshold
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LargeAssemblyStepThreshold
Parameters: largeAssemblyStepThreshold (int) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
LoadComponentsOnDemand¶
-
ViewWorkflowBuilder.
LoadComponentsOnDemand
¶ Returns or sets whether or not to load the components on demand for smart lightweight views
-------------------------------------
Getter Method
Signature
LoadComponentsOnDemand
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadComponentsOnDemand
Parameters: loadComponentsOnDemand (bool) – New in version NX11.0.0.
License requirements: drafting (“DRAFTING”)
OnLegacyViewUpdate¶
-
ViewWorkflowBuilder.
OnLegacyViewUpdate
¶ Returns or sets the on legacy view update determines whether or not components should be loaded as needed to update lightweight views
-------------------------------------
Getter Method
Signature
OnLegacyViewUpdate
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OnLegacyViewUpdate
Parameters: onLegacyViewUpdate (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
OnViewSelection¶
-
ViewWorkflowBuilder.
OnViewSelection
¶ Returns or sets the on view selection determines whether or not components should be loaded as needed for selection in lightweight views for accurate dimensioning
-------------------------------------
Getter Method
Signature
OnViewSelection
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OnViewSelection
Parameters: onViewSelection (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
PreviewStyle¶
-
ViewWorkflowBuilder.
PreviewStyle
¶ Returns or sets the style of the preview when adding a view to the drawing
-------------------------------------
Getter Method
Signature
PreviewStyle
Returns: Return type: NXOpen.Drawings.ViewWorkflowBuilderStyle
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PreviewStyle
Parameters: previewStyle ( NXOpen.Drawings.ViewWorkflowBuilderStyle
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
SelectGeometryProjectedAsArcs¶
-
ViewWorkflowBuilder.
SelectGeometryProjectedAsArcs
¶ Returns or sets the Select Geometry Projected as Arcs provides options for selection of SPLARCs entity for centerlines and Annotations
-------------------------------------
Getter Method
Signature
SelectGeometryProjectedAsArcs
Returns: Return type: NXOpen.Drawings.ViewWorkflowBuilderSplarcs
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectGeometryProjectedAsArcs
Parameters: selectGeometryProjectedAsArcs ( NXOpen.Drawings.ViewWorkflowBuilderSplarcs
) –New in version NX11.0.0.
License requirements: None.
ShowFacetEdges¶
-
ViewWorkflowBuilder.
ShowFacetEdges
¶ Returns or sets the show facet edges determines whether or not facet edges will be shown on shaded faces when displaying a drawing sheet
-------------------------------------
Getter Method
Signature
ShowFacetEdges
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowFacetEdges
Parameters: showFacetEdges (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
UseLineAntialiasing¶
-
ViewWorkflowBuilder.
UseLineAntialiasing
¶ Returns or sets the use line antialiasing
-------------------------------------
Getter Method
Signature
UseLineAntialiasing
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseLineAntialiasing
Parameters: useLineAntialiasing (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
UseTranslucency¶
-
ViewWorkflowBuilder.
UseTranslucency
¶ Returns or sets the use translucency determines translucency settings for faces when displaying a drawing sheet
-------------------------------------
Getter Method
Signature
UseTranslucency
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseTranslucency
Parameters: useTranslucency (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewWorkflowBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.