ViewWorkflowBuilderHandlingbodies Enumeration

NXOpen.Drawings.ViewWorkflowBuilder.Handlingbodies is an alias for NXOpen.Drawings.ViewWorkflowBuilderHandlingbodies

class NXOpen.Drawings.ViewWorkflowBuilderHandlingbodies

Bases: object

Represents option for handling bodies with no valid lightweight data

Deprecated since version NX9.0.3: Use NXOpen.Drawings.ViewWorkflowBuilderHandlingBodiesType instead.

Enum Members

Enum Member Enum Member Description
OmitBodiesfromView
StopUpdateandNotifyUser
StopUpdate
Generate
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.