SheetDraftingViewCollection Class¶
-
class
NXOpen.Drawings.
SheetDraftingViewCollection
¶ Bases:
object
Represents a collection of :py:class:`NXOpen.Drawings.DraftingView`s.
Use
NXOpen.Drawings.DrawingSheet.SheetDraftingViews()
to get the instance of this class.New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
CreateBaseView | For the selected part adds the base view as well as returns the reference to NXOpen.Drawings.DraftingView . |
CreateProjectedView | Lets you add a projected view (Orthoraphic View) for the selected parent view. |
DeleteView | Lets you delete the view |
FindObject | Finds the NXOpen.Drawings.DraftingView with the given identifier as recorded in a journal. |
Method Detail¶
CreateBaseView¶
-
SheetDraftingViewCollection.
CreateBaseView
¶ For the selected part adds the base view as well as returns the reference to
NXOpen.Drawings.DraftingView
.An imported model view (base view) determines orthographic space on the drawing and is used as a reference to establish the alignment and scale for all subsequent projected views.
Signature
CreateBaseView(modelView, drawingReferencePoint, viewScale, inheritClippingBoundry)
Parameters: - modelView (
NXOpen.ModelingView
) – Modeling View to be import as base view. - drawingReferencePoint (
NXOpen.Point3d
) – view origin(location) - viewScale (float) – view scale
- inheritClippingBoundry (bool) – if true inherit xyclip
Returns: Base view
Return type: New in version NX5.0.0.
License requirements: None.
- modelView (
CreateProjectedView¶
-
SheetDraftingViewCollection.
CreateProjectedView
¶ Overloaded method CreateProjectedView
CreateProjectedView(parentView, drawingReferencePoint)
CreateProjectedView(parentView, drawingReferencePoint, hingeLine)
CreateProjectedView(parentView, drawingReferencePoint, reverseDirection)
-------------------------------------
Lets you add a projected view (Orthoraphic View) for the selected parent view.
Signature
CreateProjectedView(parentView, drawingReferencePoint)
Parameters: - parentView (
NXOpen.Drawings.DraftingView
) – Selected Parent view - drawingReferencePoint (
NXOpen.Point3d
) – view origin(location)
Returns: Projected view
Return type: New in version NX5.0.0.
License requirements: None.
-------------------------------------
Lets you add a projected view (A View) for the selected parent view.
Signature
CreateProjectedView(parentView, drawingReferencePoint, hingeLine)
Parameters: - parentView (
NXOpen.Drawings.DraftingView
) – Selected Parent view - drawingReferencePoint (
NXOpen.Point3d
) – view origin(location) - hingeLine (
NXOpen.Direction
) – hinge line vector
Returns: Projected view
Return type: New in version NX5.0.0.
License requirements: None.
-------------------------------------
Lets you add a projected view (A View) for the selected parent view.
Signature
CreateProjectedView(parentView, drawingReferencePoint, reverseDirection)
Parameters: - parentView (
NXOpen.Drawings.DraftingView
) – Selected Parent view - drawingReferencePoint (
NXOpen.Point3d
) – view origin(location) - reverseDirection (bool) – reverse direction of projection
Returns: Projected view
Return type: New in version NX5.0.1.
License requirements: None.
-------------------------------------
DeleteView¶
-
SheetDraftingViewCollection.
DeleteView
¶ Lets you delete the view
Signature
DeleteView(currentView)
Parameters: currentView ( NXOpen.Drawings.DraftingView
) – View to be deletedNew in version NX5.0.0.
License requirements: None.
FindObject¶
-
SheetDraftingViewCollection.
FindObject
¶ Finds the
NXOpen.Drawings.DraftingView
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the drafting view to be found Returns: View with this identifier Return type: NXOpen.Drawings.DraftingView
New in version NX3.0.0.
License requirements: None.