SelectModelViewBuilder Class¶
-
class
NXOpen.Drawings.
SelectModelViewBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Select Model View builder that selects a model view
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
SelectedView | Returns or sets the selected view |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectedView¶
-
SelectModelViewBuilder.
SelectedView
¶ Returns or sets the selected view
-------------------------------------
Getter Method
Signature
SelectedView
Returns: Return type: NXOpen.ModelingView
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedView
Parameters: view ( NXOpen.ModelingView
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
SelectModelViewBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.