ProjectedViewBuilder Class¶
-
class
NXOpen.Drawings.
ProjectedViewBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Drawings.ProjectedView
builderTo create a new instance of this class, use
NXOpen.Drawings.DraftingViewCollection.CreateProjectedViewBuilder()
Default values.
Property Value Placement.AlignmentMethod Infer Placement.AlignmentOption ToView SecondaryComponents.ObjectType PrimaryGeometry Style.ViewStyleGeneral.AngleSetting.Angle.Value 0 Style.ViewStyleGeneral.AngleSetting.Associative 0 Style.ViewStyleGeneral.AngleSetting.EvaluationPlane DrawingSheet Style.ViewStyleGeneral.Scale.Denominator 1.0 Style.ViewStyleGeneral.Scale.Numerator 1.0 Style.ViewStyleGeneral.Scale.ScaleType Ratio Style.ViewStyleOrientation.HingeLine.ReverseDirection false Style.ViewStyleOrientation.HingeLine.VectorOption Inferred Style.ViewStyleOrientation.Ovt.AssociativeOrientation 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
HiddenObjects | Returns the list of objects to not show in the view |
NonSectionedObjects | Returns the list of objects to not section in the view |
Parent | Returns the parent view |
Placement | Returns the view position |
SecondaryComponents | Returns the list of secondary components in the view |
Style | Returns the view style |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
NonSectionedObjects¶
-
ProjectedViewBuilder.
NonSectionedObjects
¶ Returns the list of objects to not section in the view
-------------------------------------
Getter Method
Signature
NonSectionedObjects
Returns: Return type: NXOpen.Drawings.HiddenObjectsBuilder
New in version NX6.0.0.
License requirements: None.
Parent¶
-
ProjectedViewBuilder.
Parent
¶ Returns the parent view
-------------------------------------
Getter Method
Signature
Parent
Returns: Return type: NXOpen.Drawings.ParentViewBuilder
New in version NX6.0.0.
License requirements: None.
Placement¶
-
ProjectedViewBuilder.
Placement
¶ Returns the view position
-------------------------------------
Getter Method
Signature
Placement
Returns: Return type: NXOpen.Drawings.ViewPlacementBuilder
New in version NX6.0.0.
License requirements: None.
SecondaryComponents¶
-
ProjectedViewBuilder.
SecondaryComponents
¶ Returns the list of secondary components in the view
-------------------------------------
Getter Method
Signature
SecondaryComponents
Returns: Return type: NXOpen.Drawings.DraftingComponentSelectionBuilder
New in version NX11.0.0.
License requirements: None.
Style¶
-
ProjectedViewBuilder.
Style
¶ Returns the view style
-------------------------------------
Getter Method
Signature
Style
Returns: Return type: NXOpen.Drawings.ViewStyleBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ProjectedViewBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.