DrawingViewBuilder Class¶
-
class
NXOpen.Drawings.
DrawingViewBuilder
¶ Bases:
NXOpen.Builder
This builder allows the user to create a Drawing View
To create a new instance of this class, use
NXOpen.Drawings.DraftingViewCollection.CreateDrawingViewBuilder()
Default values.
Property Value MultipleViewPlacement.OptionType Center MultipleViewPlacement.ViewPlacementCenter.AlignmentMethod Infer MultipleViewPlacement.ViewPlacementCenter.AlignmentOption ToView Scale.Denominator 1.0 Scale.Numerator 1.0 Scale.ScaleType Ratio ViewStyle.ViewStyleGeneral.AngleSetting.Angle.Value 0 ViewStyle.ViewStyleGeneral.AngleSetting.Associative 0 ViewStyle.ViewStyleGeneral.AngleSetting.EvaluationPlane DrawingSheet ViewStyle.ViewStyleOrientation.HingeLine.ReverseDirection false ViewStyle.ViewStyleOrientation.HingeLine.VectorOption Inferred ViewStyle.ViewStyleOrientation.Ovt.AssociativeOrientation 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CenterCoordinate | Returns the center coordinate |
MultipleViewPlacement | Returns the multiple view placement |
Scale | Returns the view scale |
Tag | Returns the Tag for this object. |
TwodOrientation | Returns the view orientation in 2D |
ViewBoundary | Returns the view boundary. |
ViewPlacement | Returns the view placement. |
ViewStyle | Returns the view style |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CenterCoordinate¶
-
DrawingViewBuilder.
CenterCoordinate
¶ Returns the center coordinate
-------------------------------------
Getter Method
Signature
CenterCoordinate
Returns: Return type: NXOpen.Drawings.ViewCenterCoordinateBuilder
New in version NX6.0.0.
License requirements: None.
MultipleViewPlacement¶
-
DrawingViewBuilder.
MultipleViewPlacement
¶ Returns the multiple view placement
-------------------------------------
Getter Method
Signature
MultipleViewPlacement
Returns: Return type: NXOpen.Drawings.MultipleViewPlacementBuilder
New in version NX6.0.2.
License requirements: None.
Scale¶
-
DrawingViewBuilder.
Scale
¶ Returns the view scale
-------------------------------------
Getter Method
Signature
Scale
Returns: Return type: NXOpen.Drawings.ViewScaleBuilder
New in version NX6.0.0.
License requirements: None.
TwodOrientation¶
-
DrawingViewBuilder.
TwodOrientation
¶ Returns the view orientation in 2D
-------------------------------------
Getter Method
Signature
TwodOrientation
Returns: Return type: NXOpen.Drawings.View2dOrientBuilder
New in version NX6.0.0.
License requirements: None.
ViewBoundary¶
-
DrawingViewBuilder.
ViewBoundary
¶ Returns the view boundary.
It is replace by
Drawings.DrawingViewBuilder.MultipleViewPlacement()
-------------------------------------
Getter Method
Signature
ViewBoundary
Returns: Return type: NXOpen.Drawings.ViewBoundaryBuilder
New in version NX6.0.0.
Deprecated since version NX6.0.2: Use
Drawings.DrawingViewBuilder.MultipleViewPlacement()
License requirements: None.
ViewPlacement¶
-
DrawingViewBuilder.
ViewPlacement
¶ Returns the view placement.
It is replace by
Drawings.DrawingViewBuilder.MultipleViewPlacement()
-------------------------------------
Getter Method
Signature
ViewPlacement
Returns: Return type: NXOpen.Drawings.ViewPlacementBuilder
New in version NX6.0.0.
Deprecated since version NX6.0.2: Use
Drawings.DrawingViewBuilder.MultipleViewPlacement()
License requirements: None.
ViewStyle¶
-
DrawingViewBuilder.
ViewStyle
¶ Returns the view style
-------------------------------------
Getter Method
Signature
ViewStyle
Returns: Return type: NXOpen.Drawings.ViewStyleBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
DrawingViewBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.