DrawingUtils Class¶
-
class
NXOpen.
DrawingUtils
¶ Bases:
object
Contains various drawing utility methods
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX8.5.3.
Methods¶
Method | Description |
---|---|
AddDrawingAutomationWizardHandler | Registers a user defined method that is called whenever Booklet Wizard is committed. |
NewDrawingAutomationWizard | Constructs a new DrawingAutomationWizard object. |
RemoveDrawingAutomationWizardHandler | Unregisters a user defined method that is called whenever Booklet Wizard is committed. |
Method Detail¶
AddDrawingAutomationWizardHandler¶
-
DrawingUtils.
AddDrawingAutomationWizardHandler
¶ Registers a user defined method that is called whenever Booklet Wizard is committed.
Signature
AddDrawingAutomationWizardHandler(handler)
Parameters: handler (CallableObject) – method to register Returns: identifier of registered method (used to unregister the method) Return type: int New in version NX8.5.3.
License requirements: None.
NewDrawingAutomationWizard¶
-
DrawingUtils.
NewDrawingAutomationWizard
¶ Constructs a new DrawingAutomationWizard object.
Signature
NewDrawingAutomationWizard()
Returns: data for wizard callback Return type: NXOpen.Drafting.DrawingAutomationWizard
New in version NX8.5.3.
License requirements: None.
RemoveDrawingAutomationWizardHandler¶
-
DrawingUtils.
RemoveDrawingAutomationWizardHandler
¶ Unregisters a user defined method that is called whenever Booklet Wizard is committed.
Signature
RemoveDrawingAutomationWizardHandler(id)
Parameters: id (int) – identifier for method to unregister New in version NX8.5.3.
License requirements: None.