DrawingAutomationWizard Class¶
-
class
NXOpen.Drafting.
DrawingAutomationWizard
¶ Bases:
NXOpen.TransientObject
Represents callback data for the drawing automation wizard.
New in version NX8.5.3.
Properties¶
Property | Description |
---|---|
Builder | Returns or sets the drawing automation wizard builder |
ContinueProcessing | Returns or sets the flag denoting whether or not to create the booklet in the current session |
ErrorCode | Returns or sets the error code to be returned from the callback |
Part | Returns or sets the part from which the booklet drawings are created |
Property Detail¶
Builder¶
-
DrawingAutomationWizard.
Builder
¶ Returns or sets the drawing automation wizard builder
-------------------------------------
Getter Method
Signature
Builder
Returns: drawing automation wizard builder Return type: NXOpen.Drafting.DrawingCreationWizardBuilder
New in version NX8.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
Builder
Parameters: builder ( NXOpen.Drafting.DrawingCreationWizardBuilder
) – drawing automation wizard builderNew in version NX8.5.3.
License requirements: None.
ContinueProcessing¶
-
DrawingAutomationWizard.
ContinueProcessing
¶ Returns or sets the flag denoting whether or not to create the booklet in the current session
-------------------------------------
Getter Method
Signature
ContinueProcessing
Returns: flag denoting whether or not to create the booklet in the current session Return type: bool New in version NX8.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContinueProcessing
Parameters: continueProcessing (bool) – flag denoting whether or not to create the booklet in the current session New in version NX8.5.3.
License requirements: None.
ErrorCode¶
-
DrawingAutomationWizard.
ErrorCode
¶ Returns or sets the error code to be returned from the callback
-------------------------------------
Getter Method
Signature
ErrorCode
Returns: error code returned from callback Return type: int New in version NX8.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ErrorCode
Parameters: errorCode (int) – error code returned from callback New in version NX8.5.3.
License requirements: None.
Part¶
-
DrawingAutomationWizard.
Part
¶ Returns or sets the part from which the booklet drawings are created
-------------------------------------
Getter Method
Signature
Part
Returns: part from which the booklet drawings are created Return type: NXOpen.Part
New in version NX8.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
Part
Parameters: part ( NXOpen.Part
) – part from which the booklet drawings are createdNew in version NX8.5.3.
License requirements: None.
Method Detail¶
Dispose¶
-
DrawingAutomationWizard.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX8.5.3.
License requirements: None.