DraftPointDataCollection Class¶
-
class
NXOpen.
DraftPointDataCollection
¶ Bases:
object
This class contains the factory methods for creating a DraftPointData object.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateDraftPointData | Creates a DraftPointData object. |
Method Detail¶
CreateDraftPointData¶
-
DraftPointDataCollection.
CreateDraftPointData
¶ Creates a DraftPointData object.
Signature
CreateDraftPointData(point, angle)
Parameters: - point (
NXOpen.Point
) – Point Object - angle (str) – Angle value
Returns: DraftPointData Object
Return type: New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- point (