DraftPointData Class¶
-
class
NXOpen.GeometricUtilities.
DraftPointData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a draft point data object
To create an instance of this class, see
DraftPointDataCollection.CreateDraftPointData()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Parameter | Returns or sets the point coordinates |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetAngle | Returns the Angle value |
SetAngle | Sets the Angle value |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Parameter¶
-
DraftPointData.
Parameter
¶ Returns or sets the point coordinates
-------------------------------------
Getter Method
Signature
Parameter
Returns: Return type: float New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
Parameter
Parameters: parameter (float) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
GetAngle¶
-
DraftPointData.
GetAngle
¶ Returns the Angle value
Signature
GetAngle()
Returns: Angle Expression Object Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetAngle¶
-
DraftPointData.
SetAngle
¶ Sets the Angle value
Signature
SetAngle(angle)
Parameters: angle (str) – Angle string value New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
DraftPointData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.