Reflection Class¶
-
class
NXOpen.Display.
Reflection
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Display.Reflection
Reflection defines the source of reflection in shiny objects for Studio rendering style or High Quality Images.This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return None.
To create a new instance of this class, use
NXOpen.ViewCollection.CreateReflection()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Image | Returns or sets the reflections’s image builder |
ImageFilename | Returns or sets the reflection’s image filename |
ReflectionMap | Returns or sets the reflection type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ReflectionType Enumeration | where the reflections for rendering will be obtained |
Property Detail¶
Image¶
-
Reflection.
Image
¶ Returns or sets the reflections’s image builder
-------------------------------------
Getter Method
Signature
Image
Returns: Return type: NXOpen.Display.Image
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Image
Parameters: imageBuilder ( NXOpen.Display.Image
) –New in version NX5.0.0.
License requirements: None.
ImageFilename¶
-
Reflection.
ImageFilename
¶ Returns or sets the reflection’s image filename
-------------------------------------
Getter Method
Signature
ImageFilename
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageFilename
Parameters: imageFileName (str) – New in version NX5.0.0.
License requirements: None.
ReflectionMap¶
-
Reflection.
ReflectionMap
¶ Returns or sets the reflection type
-------------------------------------
Getter Method
Signature
ReflectionMap
Returns: Return type: NXOpen.Display.ReflectionType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReflectionMap
Parameters: reflectionMap ( NXOpen.Display.ReflectionType
) –New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
Reflection.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.