ReflectionType Enumeration¶
NXOpen.Display.Reflection.Type is an alias for NXOpen.Display.ReflectionType
-
class
NXOpen.Display.
ReflectionType
¶ Bases:
object
where the reflections for rendering will be obtained
Enum Members
Enum Member Enum Member Description Background use the background for reflections Stage use the stage for reflections Ibl use the image-based lighting image for reflections Image use the given image file for reflection -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-