PointCloudCollection Class¶
-
class
NXOpen.Display.
PointCloudCollection
¶ Bases:
object
Represents a collection of point cloud objects
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreatePointCloudBuilder | Creates a NXOpen.Display.PointCloudBuilder object used to build a point cloud. |
FindObject | Finds the NXOpen.Display.PointCloud with the given identifier as recorded in a journal. |
Method Detail¶
CreatePointCloudBuilder¶
-
PointCloudCollection.
CreatePointCloudBuilder
¶ Creates a
NXOpen.Display.PointCloudBuilder
object used to build a point cloud.If the referencePointCloud is not None, the referencePointCloud object will be edited.
Signature
CreatePointCloudBuilder(referencePointCloud)
Parameters: referencePointCloud ( NXOpen.Display.PointCloud
) – If referencePointCloud is not None, this object will be editedReturns: Point cloud builder Return type: NXOpen.Display.PointCloudBuilder
New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
FindObject¶
-
PointCloudCollection.
FindObject
¶ Finds the
NXOpen.Display.PointCloud
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Reference point cloud found Return type: NXOpen.Display.PointCloud
New in version NX11.0.0.
License requirements: None.