PointCloudBuilder Class¶
-
class
NXOpen.Display.
PointCloudBuilder
¶ Bases:
NXOpen.Builder
Represents a
Display.PointCloudBuilder
.:py:class:`NXOpen.Display.PointCloud`is a cloud object based on an imported point data files file (e.g. a POD file from Bentley). The point data (list of coordinates) itself won’t be stored within NX part file but an object (“Reference Point Cloud”) is created which references to the point data file and stores several meta data like clipping areas, display and current location. When loaded the point cloud will be visible as defined in the object parameters. Access to the point cloud like display, measurement, blanking/showing, sectioning, POD file loading will requires license checkout of the new basic point cloud license. For deleting a Reference Point Cloud object the license is not required.
To create a new instance of this class, use
NXOpen.Display.PointCloudCollection.CreatePointCloudBuilder()
Default values.
Property Value LoadPointDataWithPart 1 PointBrightnessMode Uniform PointColorMode Individual PointDensity 100.0 PointSize 1 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ClippingBoxesList | Returns the list of NXOpen.Display.PointCloudClippingBoxesListItemBuilder defining the clipping boxes parameters. |
LoadPointDataWithPart | Returns or sets the indication if the point cloud data will be loaded with part load. |
PointBrightnessMode | Returns or sets the point brightness display mode |
PointColorMode | Returns or sets the point color display mode |
PointDataFile | Returns or sets the point cloud data file. |
PointDensity | Returns or sets the point density |
PointSize | Returns or sets the point size |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateClippingBoxesListItemBuilder | Creates a Display.PointCloudClippingBoxesListItemBuilder . |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
LoadPointData | Loads the selected point cloud data now. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PointCloudBuilderBrightnessModes Enumeration | Specifies point cloud brightness display mode choice. |
PointCloudBuilderColorModes Enumeration | Specifies point cloud color display mode choice. |
Property Detail¶
ClippingBoxesList¶
-
PointCloudBuilder.
ClippingBoxesList
¶ Returns the list of
NXOpen.Display.PointCloudClippingBoxesListItemBuilder
defining the clipping boxes parameters.-------------------------------------
Getter Method
Signature
ClippingBoxesList
Returns: Return type: NXOpen.Display.PointCloudClippingBoxesListItemBuilderList
New in version NX11.0.0.
License requirements: None.
LoadPointDataWithPart¶
-
PointCloudBuilder.
LoadPointDataWithPart
¶ Returns or sets the indication if the point cloud data will be loaded with part load.
-------------------------------------
Getter Method
Signature
LoadPointDataWithPart
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadPointDataWithPart
Parameters: loadPointDataWithPart (bool) – New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
PointBrightnessMode¶
-
PointCloudBuilder.
PointBrightnessMode
¶ Returns or sets the point brightness display mode
-------------------------------------
Getter Method
Signature
PointBrightnessMode
Returns: Return type: NXOpen.Display.PointCloudBuilderBrightnessModes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointBrightnessMode
Parameters: pointBrightnessMode ( NXOpen.Display.PointCloudBuilderBrightnessModes
) –New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
PointColorMode¶
-
PointCloudBuilder.
PointColorMode
¶ Returns or sets the point color display mode
-------------------------------------
Getter Method
Signature
PointColorMode
Returns: Return type: NXOpen.Display.PointCloudBuilderColorModes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointColorMode
Parameters: pointColorMode ( NXOpen.Display.PointCloudBuilderColorModes
) –New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
PointDataFile¶
-
PointCloudBuilder.
PointDataFile
¶ Returns or sets the point cloud data file.
-------------------------------------
Getter Method
Signature
PointDataFile
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointDataFile
Parameters: filename (str) – New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
PointDensity¶
-
PointCloudBuilder.
PointDensity
¶ Returns or sets the point density
-------------------------------------
Getter Method
Signature
PointDensity
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointDensity
Parameters: pointDensity (float) – New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
PointSize¶
-
PointCloudBuilder.
PointSize
¶ Returns or sets the point size
-------------------------------------
Getter Method
Signature
PointSize
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSize
Parameters: pointSize (int) – New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
Method Detail¶
CreateClippingBoxesListItemBuilder¶
-
PointCloudBuilder.
CreateClippingBoxesListItemBuilder
¶ Creates a
Display.PointCloudClippingBoxesListItemBuilder
.Signature
CreateClippingBoxesListItemBuilder()
Returns: Return type: NXOpen.Display.PointCloudClippingBoxesListItemBuilder
New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
LoadPointData¶
-
PointCloudBuilder.
LoadPointData
¶ Loads the selected point cloud data now.
Signature
LoadPointData()
New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
Validate¶
-
PointCloudBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.