DatumPlaneGridBuilder Class¶
-
class
NXOpen.Display.
DatumPlaneGridBuilder
¶ Bases:
NXOpen.Display.BoundedGridBuilder
Represents the builder for adding a datum plane grid
NXOpen.Display.DatumPlaneGrid
to a datum plane.To create a new instance of this class, use
NXOpen.Display.GridCollection.CreateDatumPlaneGridBuilder()
Default values.
Property Value Associative 1 GridOrientation Custom LabelReference Local MajorLineSpacing 100 (millimeters part), 1 (inches part) MajorLineStyle Solid MajorLineWeight Normal MinorLineStyle Dashed MinorLineWeight Thin MinorLinesPerMajor 1 Show 1 ShowLabel Always ShowMajorLines 1 ShowOnTop 0 SnapPointsPerMinor 1 SnapToGrid 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative |
GridOrientation | Returns or sets the grid orientation |
LabelReference | Returns or sets the label reference |
LineColor | Returns or sets the line color |
LocalOrigin | Returns or sets the local origin |
MajorLineSpacing | Returns or sets the major line spacing |
MajorLineStyle | Returns or sets the major line style |
MajorLineWeight | Returns or sets the major line weight |
MinorLineStyle | Returns or sets the minor line style |
MinorLineWeight | Returns or sets the minor line weight |
MinorLinesPerMajor | Returns or sets the minor lines per major |
SectionCurveSettings | Returns the curve settings builder |
Show | Returns or sets the show |
ShowLabel | Returns or sets the show labels |
ShowMajorLines | Returns or sets the show major lines |
ShowOnTop | Returns or sets the show on top |
SnapPointsPerMinor | Returns or sets the snap points per minor |
SnapToGrid | Returns or sets the snap to grid |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCornerPoints | Gets corner points of the grid |
GetDatumPlanes | Get the list of datum planes. |
GetObject | Returns the object currently being edited by this builder. |
InheritSettings | Inherits the settings from the specified grid. |
SaveCurves | Creates curves by intersecting the bounded grid with all bodies in the part of the grid object. |
SetCornerPoints | Sets corner points of the grid |
SetDatumPlanes | Set the list of datum planes. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DatumPlaneGridBuilderGridOrientationType Enumeration | Specifies grid orientation option to be used for grid display. |
Property Detail¶
GridOrientation¶
-
DatumPlaneGridBuilder.
GridOrientation
¶ Returns or sets the grid orientation
-------------------------------------
Getter Method
Signature
GridOrientation
Returns: Return type: NXOpen.Display.DatumPlaneGridBuilderGridOrientationType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridOrientation
Parameters: gridOrientation ( NXOpen.Display.DatumPlaneGridBuilderGridOrientationType
) –New in version NX6.0.0.
License requirements: None.
Method Detail¶
GetDatumPlanes¶
-
DatumPlaneGridBuilder.
GetDatumPlanes
¶ Get the list of datum planes.
Signature
GetDatumPlanes()
Returns: datum plane list Return type: list of NXOpen.DatumPlane
New in version NX6.0.0.
License requirements: None.
SetDatumPlanes¶
-
DatumPlaneGridBuilder.
SetDatumPlanes
¶ Set the list of datum planes.
When editing an existing datum plane grid, only a single datum plane may be set and it must meet the following conditions: - one that currently does not have a grid associated to it - one that matches
NXOpen.Display.DatumPlaneGridBuilder.GetDatumPlanes()
Signature
SetDatumPlanes(datumPlanes)
Parameters: datumPlanes (list of NXOpen.DatumPlane
) – datum plane listNew in version NX6.0.0.
License requirements: None.
Validate¶
-
DatumPlaneGridBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.