DatumPlaneGridBuilderGridOrientationType Enumeration¶
NXOpen.Display.DatumPlaneGridBuilder.GridOrientationType is an alias for NXOpen.Display.DatumPlaneGridBuilderGridOrientationType
-
class
NXOpen.Display.
DatumPlaneGridBuilderGridOrientationType
¶ Bases:
object
Specifies grid orientation option to be used for grid display.
Enum Members
Enum Member Enum Member Description FromDatumPlane Grid display matches datum plane display Custom Grid size, location, and orientation can be customized using the manipulator controls -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-