SteelInsertSectionBuilder Class¶
-
class
NXOpen.Die.
SteelInsertSectionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Steel Insert Section sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BackSideReliefDistance | Returns the back/side relief distance of the steel insert casting |
BeltThickness | Returns the belt thickness |
ExtensionDistance | Returns the extension distance |
ExtensionType | Returns or sets the extension type |
MassLimit | Returns or sets the mass limit of the steel insert casting |
OffsetProfileToTop | Returns the offset of the profile to the top of the steel insert casting |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlanarOffsetHeight | Returns the planar contact height of the steel insert casting |
ProductContactRelief | Returns the product contact relief of the steel insert casting |
ProductContactWidth | Returns the product contact width of the steel insert casting |
ProfileRelief | Returns the profile relief |
ReliefAngle | Returns the relief angle |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetBackAttributes | Gets the back faces attributes |
GetBaseAttributes | Gets the base faces attributes |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetEndAttributes | Gets the end faces attributes |
GetFeature | Returns the feature currently being edited by this builder. |
GetFlangeWallAttributes | Gets the flange wall attributes |
GetFormingAttributes | Gets the forming faces attributes |
GetObject | Returns the object currently being edited by this builder. |
GetTrimWallAttributes | Gets the steelinsert trim wall faces attributes |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetBackAttributes | Sets the back faces attributes |
SetBackSideReliefDistance | |
SetBaseAttributes | Sets the base faces attributes |
SetBeltThickness | |
SetEndAttributes | Sets the end faces attributes |
SetExtensionDistance | |
SetFlangeWallAttributes | Sets the flange wall attributes |
SetFormingAttributes | Sets the forming faces attributes |
SetOffsetProfileToTop | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetPlanarOffsetHeight | |
SetProductContactRelief | |
SetProductContactWidth | |
SetProfileRelief | |
SetReliefAngle | |
SetTrimWallAttributes | Sets the steelinsert trim wall faces attributes |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SteelInsertSectionBuilderExtensionTypeOption Enumeration | Settings for the extension type. |
Property Detail¶
BackSideReliefDistance¶
-
SteelInsertSectionBuilder.
BackSideReliefDistance
¶ Returns the back/side relief distance of the steel insert casting
-------------------------------------
Getter Method
Signature
BackSideReliefDistance
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BeltThickness¶
-
SteelInsertSectionBuilder.
BeltThickness
¶ Returns the belt thickness
-------------------------------------
Getter Method
Signature
BeltThickness
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ExtensionDistance¶
-
SteelInsertSectionBuilder.
ExtensionDistance
¶ Returns the extension distance
-------------------------------------
Getter Method
Signature
ExtensionDistance
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ExtensionType¶
-
SteelInsertSectionBuilder.
ExtensionType
¶ Returns or sets the extension type
-------------------------------------
Getter Method
Signature
ExtensionType
Returns: Return type: NXOpen.Die.SteelInsertSectionBuilderExtensionTypeOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
ExtensionType
Parameters: extensionType ( NXOpen.Die.SteelInsertSectionBuilderExtensionTypeOption
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
MassLimit¶
-
SteelInsertSectionBuilder.
MassLimit
¶ Returns or sets the mass limit of the steel insert casting
-------------------------------------
Getter Method
Signature
MassLimit
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
MassLimit
Parameters: massLimit (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
OffsetProfileToTop¶
-
SteelInsertSectionBuilder.
OffsetProfileToTop
¶ Returns the offset of the profile to the top of the steel insert casting
-------------------------------------
Getter Method
Signature
OffsetProfileToTop
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
PlanarOffsetHeight¶
-
SteelInsertSectionBuilder.
PlanarOffsetHeight
¶ Returns the planar contact height of the steel insert casting
-------------------------------------
Getter Method
Signature
PlanarOffsetHeight
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ProductContactRelief¶
-
SteelInsertSectionBuilder.
ProductContactRelief
¶ Returns the product contact relief of the steel insert casting
-------------------------------------
Getter Method
Signature
ProductContactRelief
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ProductContactWidth¶
-
SteelInsertSectionBuilder.
ProductContactWidth
¶ Returns the product contact width of the steel insert casting
-------------------------------------
Getter Method
Signature
ProductContactWidth
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ProfileRelief¶
-
SteelInsertSectionBuilder.
ProfileRelief
¶ Returns the profile relief
-------------------------------------
Getter Method
Signature
ProfileRelief
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ReliefAngle¶
-
SteelInsertSectionBuilder.
ReliefAngle
¶ Returns the relief angle
-------------------------------------
Getter Method
Signature
ReliefAngle
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
GetBackAttributes¶
-
SteelInsertSectionBuilder.
GetBackAttributes
¶ Gets the back faces attributes
Signature
GetBackAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. title for attribute value is a str. value of attribute color is a int. color of back faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetBaseAttributes¶
-
SteelInsertSectionBuilder.
GetBaseAttributes
¶ Gets the base faces attributes
Signature
GetBaseAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. title for attribute value is a str. value of attribute color is a int. color of base faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetEndAttributes¶
-
SteelInsertSectionBuilder.
GetEndAttributes
¶ Gets the end faces attributes
Signature
GetEndAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. title for attribute value is a str. value of attribute color is a int. color of end faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetFlangeWallAttributes¶
-
SteelInsertSectionBuilder.
GetFlangeWallAttributes
¶ Gets the flange wall attributes
Signature
GetFlangeWallAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. title for attribute value is a str. value of attribute color is a int. color of flange wall faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetFormingAttributes¶
-
SteelInsertSectionBuilder.
GetFormingAttributes
¶ Gets the forming faces attributes
Signature
GetFormingAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. title for attribute value is a str. value of attribute color is a int. color of forming faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetTrimWallAttributes¶
-
SteelInsertSectionBuilder.
GetTrimWallAttributes
¶ Gets the steelinsert trim wall faces attributes
Signature
GetTrimWallAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. title for attribute value is a str. value of attribute color is a int. color of trim wall faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBackAttributes¶
-
SteelInsertSectionBuilder.
SetBackAttributes
¶ Sets the back faces attributes
Signature
SetBackAttributes(title, value, color)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of back faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBackSideReliefDistance¶
-
SteelInsertSectionBuilder.
SetBackSideReliefDistance
¶ Signature
SetBackSideReliefDistance(backSideReliefDistance)
Parameters: backSideReliefDistance (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBaseAttributes¶
-
SteelInsertSectionBuilder.
SetBaseAttributes
¶ Sets the base faces attributes
Signature
SetBaseAttributes(title, value, color)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of base faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBeltThickness¶
-
SteelInsertSectionBuilder.
SetBeltThickness
¶ Signature
SetBeltThickness(beltThickness)
Parameters: beltThickness (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetEndAttributes¶
-
SteelInsertSectionBuilder.
SetEndAttributes
¶ Sets the end faces attributes
Signature
SetEndAttributes(title, value, color)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of end faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetExtensionDistance¶
-
SteelInsertSectionBuilder.
SetExtensionDistance
¶ Signature
SetExtensionDistance(extensionDistance)
Parameters: extensionDistance (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetFlangeWallAttributes¶
-
SteelInsertSectionBuilder.
SetFlangeWallAttributes
¶ Sets the flange wall attributes
Signature
SetFlangeWallAttributes(title, value, color)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of flange wall faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetFormingAttributes¶
-
SteelInsertSectionBuilder.
SetFormingAttributes
¶ Sets the forming faces attributes
Signature
SetFormingAttributes(title, value, color)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of forming faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetOffsetProfileToTop¶
-
SteelInsertSectionBuilder.
SetOffsetProfileToTop
¶ Signature
SetOffsetProfileToTop(offsetProfileToTop)
Parameters: offsetProfileToTop (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetPlanarOffsetHeight¶
-
SteelInsertSectionBuilder.
SetPlanarOffsetHeight
¶ Signature
SetPlanarOffsetHeight(planarOffsetHeight)
Parameters: planarOffsetHeight (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetProductContactRelief¶
-
SteelInsertSectionBuilder.
SetProductContactRelief
¶ Signature
SetProductContactRelief(productContactRelief)
Parameters: productContactRelief (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetProductContactWidth¶
-
SteelInsertSectionBuilder.
SetProductContactWidth
¶ Signature
SetProductContactWidth(productContactWidth)
Parameters: productContactWidth (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetProfileRelief¶
-
SteelInsertSectionBuilder.
SetProfileRelief
¶ Signature
SetProfileRelief(profileRelief)
Parameters: profileRelief (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetReliefAngle¶
-
SteelInsertSectionBuilder.
SetReliefAngle
¶ Signature
SetReliefAngle(reliefAngle)
Parameters: reliefAngle (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetTrimWallAttributes¶
-
SteelInsertSectionBuilder.
SetTrimWallAttributes
¶ Sets the steelinsert trim wall faces attributes
Signature
SetTrimWallAttributes(title, value, color)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of trim wall faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
SteelInsertSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.