QuickBinderWrapBuilder Class¶
-
class
NXOpen.Die.
QuickBinderWrapBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Die.QuickBinderWrapBuilder
builderThis is an abstract class, and cannot be created.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Button | Returns the button |
ChangeRadius | Returns the change radius value |
EditSizeChoice | Returns or sets the edit size choice |
Matrix | Returns or sets the rotation matrix |
Origin | Returns or sets the origin |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the method |
UMaximum | Returns the maximum U value |
UMinimum | Returns the minumum U value |
VMaximum | Returns the maximum V value |
VMinimum | Returns the minumum V value |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
QuickBinderWrapBuilderEditSizeType Enumeration | Settings for the edit size type. |
QuickBinderWrapBuilderTypes Enumeration | Settings for the binder wrap sheet body type. |
Property Detail¶
Button¶
-
QuickBinderWrapBuilder.
Button
¶ Returns the button
-------------------------------------
Getter Method
Signature
Button
Returns: Return type: NXOpen.SelectBodyList
New in version NX5.0.0.
License requirements: None.
ChangeRadius¶
-
QuickBinderWrapBuilder.
ChangeRadius
¶ Returns the change radius value
-------------------------------------
Getter Method
Signature
ChangeRadius
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
EditSizeChoice¶
-
QuickBinderWrapBuilder.
EditSizeChoice
¶ Returns or sets the edit size choice
-------------------------------------
Getter Method
Signature
EditSizeChoice
Returns: Return type: NXOpen.Die.QuickBinderWrapBuilderEditSizeType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EditSizeChoice
Parameters: sizeChoice ( NXOpen.Die.QuickBinderWrapBuilderEditSizeType
) –New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Matrix¶
-
QuickBinderWrapBuilder.
Matrix
¶ Returns or sets the rotation matrix
-------------------------------------
Getter Method
Signature
Matrix
Returns: Return type: NXOpen.Matrix3x3
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Matrix
Parameters: matrix ( NXOpen.Matrix3x3
) –New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Origin¶
-
QuickBinderWrapBuilder.
Origin
¶ Returns or sets the origin
-------------------------------------
Getter Method
Signature
Origin
Returns: Return type: NXOpen.Point3d
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Origin
Parameters: origin ( NXOpen.Point3d
) –New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Type¶
-
QuickBinderWrapBuilder.
Type
¶ Returns or sets the method
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Die.QuickBinderWrapBuilderTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Die.QuickBinderWrapBuilderTypes
) –New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
UMaximum¶
-
QuickBinderWrapBuilder.
UMaximum
¶ Returns the maximum U value
-------------------------------------
Getter Method
Signature
UMaximum
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
UMinimum¶
-
QuickBinderWrapBuilder.
UMinimum
¶ Returns the minumum U value
-------------------------------------
Getter Method
Signature
UMinimum
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
VMaximum¶
-
QuickBinderWrapBuilder.
VMaximum
¶ Returns the maximum V value
-------------------------------------
Getter Method
Signature
VMaximum
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
VMinimum¶
-
QuickBinderWrapBuilder.
VMinimum
¶ Returns the minumum V value
-------------------------------------
Getter Method
Signature
VMinimum
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
QuickBinderWrapBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.