LineupBuilder Class¶
-
class
NXOpen.Die.
LineupBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Lineup feature builder
To create a new instance of this class, use
NXOpen.Die.DieCollection.Lineup()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
FlowDirection | Returns or sets the flow direction of the lineup |
Origin | Returns or sets the origin of the lineup |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PressDirection | Returns or sets the press direction of the lineup |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDetails | Gets the detailed description of the lineup |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetProductBodies | Gets the product sheet bodies of the lineup |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetDetails | Sets the detailed description of the lineup |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetProductBodies | Sets the product sheet bodies of the lineup |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FlowDirection¶
-
LineupBuilder.
FlowDirection
¶ Returns or sets the flow direction of the lineup
-------------------------------------
Getter Method
Signature
FlowDirection
Returns: Return type: NXOpen.Vector3d
New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
FlowDirection
Parameters: flowDirection ( NXOpen.Vector3d
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Origin¶
-
LineupBuilder.
Origin
¶ Returns or sets the origin of the lineup
-------------------------------------
Getter Method
Signature
Origin
Returns: Return type: NXOpen.Point3d
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
Origin
Parameters: origin ( NXOpen.Point3d
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
PressDirection¶
-
LineupBuilder.
PressDirection
¶ Returns or sets the press direction of the lineup
-------------------------------------
Getter Method
Signature
PressDirection
Returns: Return type: NXOpen.Vector3d
New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
PressDirection
Parameters: pressDirection ( NXOpen.Vector3d
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Method Detail¶
GetDetails¶
-
LineupBuilder.
GetDetails
¶ Gets the detailed description of the lineup
Signature
GetDetails()
Returns: detail strings Return type: list of str New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetProductBodies¶
-
LineupBuilder.
GetProductBodies
¶ Gets the product sheet bodies of the lineup
Signature
GetProductBodies()
Returns: Return type: list of NXOpen.Body
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetDetails¶
-
LineupBuilder.
SetDetails
¶ Sets the detailed description of the lineup
Signature
SetDetails(strings)
Parameters: strings (list of str) – detail strings New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetProductBodies¶
-
LineupBuilder.
SetProductBodies
¶ Sets the product sheet bodies of the lineup
Signature
SetProductBodies(objects)
Parameters: objects (list of NXOpen.Body
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Validate¶
-
LineupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.