DieBooleanBuilder Class¶
-
class
NXOpen.Die.
DieBooleanBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Die.DieBooleanBuilder
.This class is a helper to other Die Design features that identify specific booleans in their dialogs, such as the Die Shoe feature.
To create a new instance of this class, use
NXOpen.Die.DieCollection.CreateDieBoolean()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BooleanOptions | Returns or sets the boolean option to apply to the list of selected solids |
SelectBodies | Returns the bodies to be booleaned to the main feature body |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DieBooleanBuilderBooleanType Enumeration | boolean type to apply to the selected solids |
Property Detail¶
BooleanOptions¶
-
DieBooleanBuilder.
BooleanOptions
¶ Returns or sets the boolean option to apply to the list of selected solids
-------------------------------------
Getter Method
Signature
BooleanOptions
Returns: Return type: NXOpen.Die.DieBooleanBuilderBooleanType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BooleanOptions
Parameters: booleanOptions ( NXOpen.Die.DieBooleanBuilderBooleanType
) –New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
SelectBodies¶
-
DieBooleanBuilder.
SelectBodies
¶ Returns the bodies to be booleaned to the main feature body
-------------------------------------
Getter Method
Signature
SelectBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
DieBooleanBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.