DieBooleanBuilderBooleanType Enumeration¶
NXOpen.Die.DieBooleanBuilder.BooleanType is an alias for NXOpen.Die.DieBooleanBuilderBooleanType
-
class
NXOpen.Die.
DieBooleanBuilderBooleanType
¶ Bases:
object
boolean type to apply to the selected solids
Enum Members
Enum Member Enum Member Description Unite Unite the solids to the application solid. Subtract Subtract the solids from the application solid. Intersect Intersect the solids with the application solid. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-