TableSettingsBuilder Class¶
-
class
NXOpen.Diagramming.Tables.
TableSettingsBuilder
¶ Bases:
NXOpen.Diagramming.BaseTaggedObjectBuilder
Represents a TableSettingsBuilder.
This is a sub-builder class and cannot be directly instantiated
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AnchorLocation | Returns or sets the anchor location of the table settings. |
HeaderLocation | Returns or sets the header location of the table settings. |
HeaderOrientation | Returns or sets the header orientation of the table settings. |
ProtectedFlag | Returns or sets the protected flag. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AnchorLocation¶
-
TableSettingsBuilder.
AnchorLocation
¶ Returns or sets the anchor location of the table settings.
-------------------------------------
Getter Method
Signature
AnchorLocation
Returns: Return type: NXOpen.Diagramming.Tables.AnchorLocation
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnchorLocation
Parameters: anchorLocation ( NXOpen.Diagramming.Tables.AnchorLocation
) –New in version NX10.0.0.
License requirements: None.
HeaderLocation¶
-
TableSettingsBuilder.
HeaderLocation
¶ Returns or sets the header location of the table settings.
-------------------------------------
Getter Method
Signature
HeaderLocation
Returns: Return type: NXOpen.Diagramming.Tables.HeaderLocation
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeaderLocation
Parameters: headerLocation ( NXOpen.Diagramming.Tables.HeaderLocation
) –New in version NX10.0.0.
License requirements: None.
HeaderOrientation¶
-
TableSettingsBuilder.
HeaderOrientation
¶ Returns or sets the header orientation of the table settings.
-------------------------------------
Getter Method
Signature
HeaderOrientation
Returns: Return type: NXOpen.Diagramming.Tables.HeaderOrientation
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeaderOrientation
Parameters: headerOrientation ( NXOpen.Diagramming.Tables.HeaderOrientation
) –New in version NX10.0.0.
License requirements: None.
ProtectedFlag¶
-
TableSettingsBuilder.
ProtectedFlag
¶ Returns or sets the protected flag.
-------------------------------------
Getter Method
Signature
ProtectedFlag
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProtectedFlag
Parameters: flag (bool) – New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
TableSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.