BaseTaggedObjectBuilder Class

class NXOpen.Diagramming.BaseTaggedObjectBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a BaseTaggedObjectBuilder.

This is an abstract and sub-builder class and cannot be directly instantiated

New in version NX10.0.0.

Properties

Property Description
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Method Detail

Validate

BaseTaggedObjectBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.