ContinuationDataBuilder Class¶
-
class
NXOpen.Diagramming.Tables.
ContinuationDataBuilder
¶ Bases:
NXOpen.Diagramming.BaseTaggedObjectBuilder
Represents a ContinuationDataBuilder.
This is a sub-builder class and cannot be directly instantiated
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Location | Returns or sets the location to continue a table if it won’t fit. |
MaximumSize | Returns or sets the maximum size of any section of a table. |
Spacing | Returns or sets the spacing between sections of a table. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Location¶
-
ContinuationDataBuilder.
Location
¶ Returns or sets the location to continue a table if it won’t fit.
-------------------------------------
Getter Method
Signature
Location
Returns: Return type: NXOpen.Diagramming.Tables.ContinuationLocation
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Location
Parameters: location ( NXOpen.Diagramming.Tables.ContinuationLocation
) –New in version NX10.0.0.
License requirements: None.
MaximumSize¶
-
ContinuationDataBuilder.
MaximumSize
¶ Returns or sets the maximum size of any section of a table.
-------------------------------------
Getter Method
Signature
MaximumSize
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumSize
Parameters: maximumSize (float) – New in version NX10.0.0.
License requirements: None.
Spacing¶
-
ContinuationDataBuilder.
Spacing
¶ Returns or sets the spacing between sections of a table.
-------------------------------------
Getter Method
Signature
Spacing
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Spacing
Parameters: spacing (float) – New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ContinuationDataBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.