CellSettingsBuilder Class¶
-
class
NXOpen.Diagramming.Tables.
CellSettingsBuilder
¶ Bases:
NXOpen.Diagramming.BaseTaggedObjectBuilder
Represents a CellSettingsBuilder.
This is a sub-builder class and cannot be directly instantiated
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ContentAlignment | Returns or sets the content alignment of the cell settings. |
FillColor | Returns or sets the fill color. |
FillOpacity | Returns or sets the fill opacity. |
OverflowBehavior | Returns or sets the overflow behavior of the cell settings. |
Tag | Returns the Tag for this object. |
ZeroDisplay | Returns or sets the zero display of the cell settings. |
Methods¶
Method | Description |
---|---|
GetContentTextStyle | Gets context text style . |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ContentAlignment¶
-
CellSettingsBuilder.
ContentAlignment
¶ Returns or sets the content alignment of the cell settings.
-------------------------------------
Getter Method
Signature
ContentAlignment
Returns: Return type: NXOpen.Diagramming.Tables.ContentAlignment
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContentAlignment
Parameters: contentAlignment ( NXOpen.Diagramming.Tables.ContentAlignment
) –New in version NX10.0.0.
License requirements: None.
FillColor¶
-
CellSettingsBuilder.
FillColor
¶ Returns or sets the fill color.
-------------------------------------
Getter Method
Signature
FillColor
Returns: Return type: Id New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FillColor
Parameters: colorId (Id) – New in version NX10.0.0.
License requirements: None.
FillOpacity¶
-
CellSettingsBuilder.
FillOpacity
¶ Returns or sets the fill opacity.
The range of opacity is from 0.0 to 1.0. 0.0 is completely transparent and 1.0 is completely opaque.
-------------------------------------
Getter Method
Signature
FillOpacity
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FillOpacity
Parameters: opacity (float) – New in version NX10.0.0.
License requirements: None.
OverflowBehavior¶
-
CellSettingsBuilder.
OverflowBehavior
¶ Returns or sets the overflow behavior of the cell settings.
-------------------------------------
Getter Method
Signature
OverflowBehavior
Returns: Return type: NXOpen.Diagramming.Tables.OverflowBehavior
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverflowBehavior
Parameters: overflowBehavior ( NXOpen.Diagramming.Tables.OverflowBehavior
) –New in version NX10.0.0.
License requirements: None.
ZeroDisplay¶
-
CellSettingsBuilder.
ZeroDisplay
¶ Returns or sets the zero display of the cell settings.
-------------------------------------
Getter Method
Signature
ZeroDisplay
Returns: Return type: NXOpen.Diagramming.Tables.ZeroDisplay
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZeroDisplay
Parameters: zeroDisplay ( NXOpen.Diagramming.Tables.ZeroDisplay
) –New in version NX10.0.0.
License requirements: None.
Method Detail¶
GetContentTextStyle¶
-
CellSettingsBuilder.
GetContentTextStyle
¶ Gets context text style .
Signature
GetContentTextStyle()
Returns: Return type: NXOpen.Diagramming.TextStyleBuilder
New in version NX11.0.1.
License requirements: None.
Validate¶
-
CellSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.