CellRangeBuilder Class¶
-
class
NXOpen.Diagramming.Tables.
CellRangeBuilder
¶ Bases:
NXOpen.Diagramming.BaseTaggedObjectBuilder
Represents a CellRangeBuilder.
This is a sub-builder class and cannot be directly instantiated
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
CanHide | Returns or sets the can hide flag. |
Hidden | Returns or sets the hidden flag. |
Size | Returns or sets the size. |
SizingMethod | Returns or sets the sizing method. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CanHide¶
-
CellRangeBuilder.
CanHide
¶ Returns or sets the can hide flag.
-------------------------------------
Getter Method
Signature
CanHide
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanHide
Parameters: canHide (bool) – New in version NX10.0.0.
License requirements: None.
Size¶
-
CellRangeBuilder.
Size
¶ Returns or sets the size.
-------------------------------------
Getter Method
Signature
Size
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Size
Parameters: size (float) – New in version NX10.0.0.
License requirements: None.
SizingMethod¶
-
CellRangeBuilder.
SizingMethod
¶ Returns or sets the sizing method.
-------------------------------------
Getter Method
Signature
SizingMethod
Returns: Return type: NXOpen.Diagramming.Tables.SizingMethod
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SizingMethod
Parameters: sizingMethod ( NXOpen.Diagramming.Tables.SizingMethod
) –New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CellRangeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.